PFE_MAC1 and GMAC0 is not working with the GoldVIP Linux image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFE_MAC1 and GMAC0 is not working with the GoldVIP Linux image

ソリューションへジャンプ
1,386件の閲覧回数
salimmulla2021
Contributor III

I have flashed image fsl-image-goldvip-s32g274ardb2.sdcard provided by the NXP as part of GoldVIP Package on the SD card and after that when tried to test the 1. P3A (GMAC0) and P5 (PFE_MAC1 ) interface got the following issues :

1. P3A : Link is getting up (Led’s are blinking) But not able to find the interface in /etc/network/interface file. 2. P5 : While making the PFE1 interface down and up with the command ifconfig pfe1 up/down getting the error message as root@s32g274ardb2[ 296.429966] phy-s32gen1-serdes 44180000.serdes: Speed not supported. :[ 296.431117] phy-s32gen1-serdes 44180000.serdes: Speed not supported. Request you to provide the inputs.

タグ(2)
0 件の賞賛
返信
1 解決策
1,362件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are seeing that you also submit a ticket under the NXP online services. You are being supported inside the platform.

Do you require for the information to be mirrored into this case?

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,348件の閲覧回数
salimmulla2021
Contributor III

You can close this.

0 件の賞賛
返信
1,363件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are seeing that you also submit a ticket under the NXP online services. You are being supported inside the platform.

Do you require for the information to be mirrored into this case?

Please, let us know.

0 件の賞賛
返信