PFE_MAC1 and GMAC0 is not working with the GoldVIP Linux image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PFE_MAC1 and GMAC0 is not working with the GoldVIP Linux image

Jump to solution
1,256 Views
salimmulla2021
Contributor III

I have flashed image fsl-image-goldvip-s32g274ardb2.sdcard provided by the NXP as part of GoldVIP Package on the SD card and after that when tried to test the 1. P3A (GMAC0) and P5 (PFE_MAC1 ) interface got the following issues :

1. P3A : Link is getting up (Led’s are blinking) But not able to find the interface in /etc/network/interface file. 2. P5 : While making the PFE1 interface down and up with the command ifconfig pfe1 up/down getting the error message as root@s32g274ardb2[ 296.429966] phy-s32gen1-serdes 44180000.serdes: Speed not supported. :[ 296.431117] phy-s32gen1-serdes 44180000.serdes: Speed not supported. Request you to provide the inputs.

Tags (2)
0 Kudos
Reply
1 Solution
1,232 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are seeing that you also submit a ticket under the NXP online services. You are being supported inside the platform.

Do you require for the information to be mirrored into this case?

Please, let us know.

View solution in original post

0 Kudos
Reply
2 Replies
1,218 Views
salimmulla2021
Contributor III

You can close this.

0 Kudos
Reply
1,233 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are seeing that you also submit a ticket under the NXP online services. You are being supported inside the platform.

Do you require for the information to be mirrored into this case?

Please, let us know.

0 Kudos
Reply