The kernel driver for PCA85073A RTC is defined in rtc-pcf85063.c. The respective configuration option is CONFIG_RTC_DRV_PCF85063. The driver is enabled in Automotive BSP kernel by default.
Best Regards,
Platon
Hi ,
i tried but boot log showing below mentioned error
2.984709] 001: rtc-pcf85063 0-0051: RTC chip is not present
[ 2.984794] 001: rtc-pcf85063: probe of 0-0051 failed with error -110
Hi ,
i am working with NXP S32g274a our custom development board. and BSP version 29.0.0
Suggestions:
1. Make sure the RTC responds to the access cycles on the I2C bus it is
connected to.
2. Make sure the connection between the RTC and the central chip is properly
reflected in the Device Tree
Best Regards,
Platon
Hi ,
This is my device tree for pca85073a. if you want any changes in dtsi. please point out your idea.
&i2c1 {
status = "okay";
clock-frequency = <100000>;
rtc@51 {
compatible = "nxp,pca85073a";
reg = <0x51>;
nxp,no-battery;
};
};
Thanks
Vimal
Hi ,
still iam facing issue with i2c-1 for below Mentioned Pin
pinctrl1_i2c1: i2c1grp {
fsl,pins = <
S32_GEN1_PAD_PB3__I2C1_SCLK_OUT
S32_GEN1_PAD_PB4__I2C1_DATA_OUT
S32_GEN1_PAD_PB3__I2C1_SCLK_IN
S32_GEN1_PAD_PB4__I2C1_DATA_IN
>;
};
pinctrl_gpioeirq: gpioeirqgrp {
fsl,pins = <
//S32_GEN1_PAD_PB3__SIUL_EIRQ0
S32_GEN1_PAD_PB4__SIUL_EIRQ1
Hi ,
same RTC(85073) module work with other i2c. but i2c-1 (PB3,PB4) pins are not working. could you give me any solutions.
Thanks
vimal