NXPS32G3 support for android porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXPS32G3 support for android porting

215 Views
soundharya
Contributor I

Hi team,

We would like to know if it is possible to port android image in nxps32g399 board.

As we came across the porting of android can be done only on NXP i.MX processors.

Requesting to confirm if it is possible or not possible to port android in NXPS32g399 board without support of any other hardware?

 

Thank you

Tags (1)
0 Kudos
Reply
1 Reply

180 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @soundharya 

Thanks for your post.

Officially, the S32G family provide Linux BSP for working with the A53 cores, we do not offer any kind of support for Android, also, there is not any example or documentation on how to port it.

Theoretically, it is possible to use the Android on the S32G board, If you would like to perform the Android port to the S32G3, it may have to be done by yourself

Sorry for your inconvenience.

 

BR

Chenyin

0 Kudos
Reply