Maximum sustained force for heat sink attachment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum sustained force for heat sink attachment

ソリューションへジャンプ
1,067件の閲覧回数
Cooper8121
Contributor I

Hi all,

What's definition of maximum force in Table 5. Maximum force for common Freescale packages.

https://www.nxp.com/docs/en/application-note/AN4871.pdf

Is it sustained force?

Thanks.

Cooper.

 

0 件の賞賛
1 解決策
1,059件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Yes, this is the maximum sustained force that can be continuously applied to the top of the package.

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,060件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Yes, this is the maximum sustained force that can be continuously applied to the top of the package.

0 件の賞賛