Hi,
I am working on S32G-VNP-EVB board. i have compiled a sample binary using S32DS3.4 to glow led using rtc example, which runs on M7.
S32G Debug probe:
From S32G Debug probe when connected to target, ELF is working.
Application Bootloader:
Application bootloader is created as a raw binary with below address.
0x3400C000
In Linker file, made below changes as 8MB SRAM is there on EVB.
From u-boot initialized SRAM using below command.
initsram 0x34000000
ext4load mmc 0:2 0x3400c000 /boot/blob.bin
startm7 0x3400c000 //Tried with reset_handler address also//
After this LED is not glowing, which confirms image is not starting.
Clarification: Please provide the correct linker file for EVB.
IVT + DCD + App Binary should be copied to SDCARD and run from SRAM.
Please provide us the correct DCD to be used for this process.
Thanks in advance.
Hi,
Have you solve this problem? I have the same,but i have no idea to clear it.
Can you help me?
Best Regards!