Location of Platform_Software_Integration for s32g3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Location of Platform_Software_Integration for s32g3

Jump to solution
419 Views
Niranj_369
Contributor I

Hi

I'm working on booting a53 and m7 cores of s32g3 soc parallely. Im following  the AN13750 document. In the document the below file is mentioned

Platform_Software_Integration_S32G2_2022_06.exe

Niranj_369_0-1759498697218.png

Where can i find this file for s32g3 soc.

Tags (1)
0 Kudos
Reply
1 Solution
402 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for the post.

1. For S32G3, there are two versions existed, you may find it from your NXP account

chenyin_h_0-1759501813310.png

2. But currently, the "Integration Reference Examples" is end of support, if you are willing to try the M7 bootloader, newer version projects are provided within the GoldVIP package, you may reference the GoldVIP for details.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
3 Replies
329 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for your reply,

It is the flexnet link, commonly it is only available for your when you had logged to the NXP.com. 

If you are searching for the certain package within your account, you may find the package from the list, or try searching it the following way when logged in with your NXP account.

chenyin_h_0-1759669429410.png

 

BR

Chenyin

0 Kudos
Reply
403 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for the post.

1. For S32G3, there are two versions existed, you may find it from your NXP account

chenyin_h_0-1759501813310.png

2. But currently, the "Integration Reference Examples" is end of support, if you are willing to try the M7 bootloader, newer version projects are provided within the GoldVIP package, you may reference the GoldVIP for details.

 

BR

Chenyin

0 Kudos
Reply
364 Views
Niranj_369
Contributor I

Hi @chenyin_h 

I tried to access the page using the below link  but it redirects to the nxp profile page. Yesterday it was working for sometime.
https://nxp.flexnetoperations.com/control/frse/product?child_plneID=854617&cert_num=206694071

0 Kudos
Reply