Location of Platform_Software_Integration for s32g3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Location of Platform_Software_Integration for s32g3

ソリューションへジャンプ
428件の閲覧回数
Niranj_369
Contributor I

Hi

I'm working on booting a53 and m7 cores of s32g3 soc parallely. Im following  the AN13750 document. In the document the below file is mentioned

Platform_Software_Integration_S32G2_2022_06.exe

Niranj_369_0-1759498697218.png

Where can i find this file for s32g3 soc.

タグ(1)
0 件の賞賛
返信
1 解決策
411件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for the post.

1. For S32G3, there are two versions existed, you may find it from your NXP account

chenyin_h_0-1759501813310.png

2. But currently, the "Integration Reference Examples" is end of support, if you are willing to try the M7 bootloader, newer version projects are provided within the GoldVIP package, you may reference the GoldVIP for details.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
338件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for your reply,

It is the flexnet link, commonly it is only available for your when you had logged to the NXP.com. 

If you are searching for the certain package within your account, you may find the package from the list, or try searching it the following way when logged in with your NXP account.

chenyin_h_0-1759669429410.png

 

BR

Chenyin

0 件の賞賛
返信
412件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Niranj_369 

Thanks for the post.

1. For S32G3, there are two versions existed, you may find it from your NXP account

chenyin_h_0-1759501813310.png

2. But currently, the "Integration Reference Examples" is end of support, if you are willing to try the M7 bootloader, newer version projects are provided within the GoldVIP package, you may reference the GoldVIP for details.

 

BR

Chenyin

0 件の賞賛
返信
373件の閲覧回数
Niranj_369
Contributor I

Hi @chenyin_h 

I tried to access the page using the below link  but it redirects to the nxp profile page. Yesterday it was working for sometime.
https://nxp.flexnetoperations.com/control/frse/product?child_plneID=854617&cert_num=206694071

0 件の賞賛
返信