LLCE_LIN Build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE_LIN Build error

Jump to solution
4,537 Views
Subramanya_Holla
Contributor I

Hello NXP, I'm currently working with the LIN LLCE demo package you provided. Despite following the instructions in the description file, I've run into an error. Could you please assist me in resolving it? I've also tried manually adding the path of CDD_Rm.h in the properties -> settings -> tool settings -> includes -> include_paths, but I'm still encountering additional errors afterward.
MicrosoftTeams-image (28).png

0 Kudos
Reply
1 Solution
4,514 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. Given the package versions, it seems that the following thread talks about the same issue:

Solved: LLCE_LIN S32G-VNP-RDB2 - NXP Community

A solution was provided under the above community thread. You should be able to run the example correctly following the explained steps. We apologize for the inconvenience.

Please, let us know.

View solution in original post

0 Kudos
Reply
4 Replies
4,518 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which RTD/LLCE versions are you using?

Have you modified anything of the example itself?

Please, let us know.

0 Kudos
Reply
4,517 Views
Subramanya_Holla
Contributor I

FYI Im using S32DS 3.5.3, RTD 4.0.2 and LLCE 1.0.7.

No I haven't modified anything from the example.

0 Kudos
Reply
4,515 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. Given the package versions, it seems that the following thread talks about the same issue:

Solved: LLCE_LIN S32G-VNP-RDB2 - NXP Community

A solution was provided under the above community thread. You should be able to run the example correctly following the explained steps. We apologize for the inconvenience.

Please, let us know.

0 Kudos
Reply
1,534 Views
Subramanya_Holla
Contributor I

Hello Daniel Aguirre,

I wanted to express my gratitude for your assistance. The thread you shared proved invaluable in resolving the issue I encountered while building the code. Additionally, I successfully tested the transmission and reception functions of LIN in CANoe, as depicted in the image below. However, I am curious about how this demo validates LIN LLCE. I haven't come across any code pertaining to LLCE routing. Could you provide guidance on how to test LLCE LIN routing? Any help would be greatly appreciated.
llce_Lin.png

0 Kudos
Reply