Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

跳至解决方案
1,458 次查看
vigneshrk0482
Contributor II

I have powered on the NXP S32G RDB2 Board and was able to communicate serially with PuTTY.  However when I want to connect ethernet cable to it. Even though I tried assigning static IPs, it wouldn't ping. I want to enable the ethernet driver or solve the issue so that I can test my usecases.

标记 (3)
0 项奖励
回复
1 解答
1,409 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for your reply.

I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly.

The testing log is attached for your reference.

 

BR

Chenyin

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,380 次查看
vigneshrk0482
Contributor II

Hello @chenyin_h , I am glad to share that finally it is pinging and tested out by connecting to router and creating a private network with other boards, for now I am exploring ethernet communications at other ports too. For any other problems, I shall open another ticket or post.

Thank you!

0 项奖励
回复
1,410 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for your reply.

I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly.

The testing log is attached for your reference.

 

BR

Chenyin

0 项奖励
回复
1,435 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for the post.

May I know which version BSP(or other software package) is used for your test? which network port was used?

 

BR

Chenyin 

0 项奖励
回复
1,430 次查看
vigneshrk0482
Contributor II

Hello @chenyin_h ,

The BSP version is Auto Linux 35 (U-boot from SD Card) and using the GMAC port. However I think that the ethernet is not enabled. When I checked eth0 in ip route it says NO-CARRIER but in ifconfig it says UP. Also I want to use this to communicate with Raspberry Pi to NXP board. Please guide me what steps to do as I have tried all the attempts.

标记 (3)
0 项奖励
回复