Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

Jump to solution
1,108 Views
vigneshrk0482
Contributor II

I have powered on the NXP S32G RDB2 Board and was able to communicate serially with PuTTY.  However when I want to connect ethernet cable to it. Even though I tried assigning static IPs, it wouldn't ping. I want to enable the ethernet driver or solve the issue so that I can test my usecases.

Tags (3)
0 Kudos
Reply
1 Solution
1,059 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for your reply.

I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly.

The testing log is attached for your reference.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
4 Replies
1,030 Views
vigneshrk0482
Contributor II

Hello @chenyin_h , I am glad to share that finally it is pinging and tested out by connecting to router and creating a private network with other boards, for now I am exploring ethernet communications at other ports too. For any other problems, I shall open another ticket or post.

Thank you!

0 Kudos
Reply
1,060 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for your reply.

I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly.

The testing log is attached for your reference.

 

BR

Chenyin

0 Kudos
Reply
1,085 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @vigneshrk0482 

Thanks for the post.

May I know which version BSP(or other software package) is used for your test? which network port was used?

 

BR

Chenyin 

0 Kudos
Reply
1,080 Views
vigneshrk0482
Contributor II

Hello @chenyin_h ,

The BSP version is Auto Linux 35 (U-boot from SD Card) and using the GMAC port. However I think that the ethernet is not enabled. When I checked eth0 in ip route it says NO-CARRIER but in ifconfig it says UP. Also I want to use this to communicate with Raspberry Pi to NXP board. Please guide me what steps to do as I have tried all the attempts.

Tags (3)
0 Kudos
Reply