Is there a POR analog module inside S32G2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a POR analog module inside S32G2?

ソリューションへジャンプ
1,158件の閲覧回数
brian_w
Contributor III

Hi,

Inside S32G2, except the CSPD, Is there a POR analog module? If yes, what's the difference between  the function of POR and the function SPD?

From the following figure, there seems to be a individual POR ananlog module except CSPD, but I can not find the clear description in the RM.

brian_w_0-1675922284004.png

 

0 件の賞賛
返信
1 解決策
1,144件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For your question, we assume analog modules is referred to internal voltage monitoring.

The following is said in S32G2 RM [Page 1204, S32G2 Reference Manual, Rev. 6, 11/2022]:

"There are no on-chip precision voltage monitors. All required precision voltage monitoring is done off-chip. Each precision voltage
monitor should be on the same sense point as the regulator for the corresponding power supply."

Please, let us know if this information was helpful or not.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,145件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For your question, we assume analog modules is referred to internal voltage monitoring.

The following is said in S32G2 RM [Page 1204, S32G2 Reference Manual, Rev. 6, 11/2022]:

"There are no on-chip precision voltage monitors. All required precision voltage monitoring is done off-chip. Each precision voltage
monitor should be on the same sense point as the regulator for the corresponding power supply."

Please, let us know if this information was helpful or not.

0 件の賞賛
返信
1,133件の閲覧回数
brian_w
Contributor III

Hi,

Thank you for your reply.

 

0 件の賞賛
返信