Is there a POR analog module inside S32G2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a POR analog module inside S32G2?

Jump to solution
1,094 Views
brian_w
Contributor III

Hi,

Inside S32G2, except the CSPD, Is there a POR analog module? If yes, what's the difference between  the function of POR and the function SPD?

From the following figure, there seems to be a individual POR ananlog module except CSPD, but I can not find the clear description in the RM.

brian_w_0-1675922284004.png

 

0 Kudos
Reply
1 Solution
1,080 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For your question, we assume analog modules is referred to internal voltage monitoring.

The following is said in S32G2 RM [Page 1204, S32G2 Reference Manual, Rev. 6, 11/2022]:

"There are no on-chip precision voltage monitors. All required precision voltage monitoring is done off-chip. Each precision voltage
monitor should be on the same sense point as the regulator for the corresponding power supply."

Please, let us know if this information was helpful or not.

View solution in original post

0 Kudos
Reply
2 Replies
1,081 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For your question, we assume analog modules is referred to internal voltage monitoring.

The following is said in S32G2 RM [Page 1204, S32G2 Reference Manual, Rev. 6, 11/2022]:

"There are no on-chip precision voltage monitors. All required precision voltage monitoring is done off-chip. Each precision voltage
monitor should be on the same sense point as the regulator for the corresponding power supply."

Please, let us know if this information was helpful or not.

0 Kudos
Reply
1,069 Views
brian_w
Contributor III

Hi,

Thank you for your reply.

 

0 Kudos
Reply