Is the S32G2-VNP-RDB2 board compatible with the auto_yocto_bsp ubuntu image?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the S32G2-VNP-RDB2 board compatible with the auto_yocto_bsp ubuntu image?

802 次查看
Gerry15
Contributor III

Hello,

 

I already use the auto_yocto_bsp for running the S32G-VNP-RDB2 development board, but I always build the image with the normal -m "non-ubuntu" option. There is also the option to build the image with ubuntu(-base), would this work on this board?  

标记 (3)
0 项奖励
回复
4 回复数

787 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Besides it works, we don;t recommend to use the ubuntu mage since all features included in yocto for auto will lost.

Regards

 

0 项奖励
回复

774 次查看
Gerry15
Contributor III

Hey,

thank you for the quick answer. What are the auto features concretely? Further, what is the difference between `fsl-image-ubuntu` `fsl-image-ubuntu-base`? 
P.S. what is the standard login for 'fsl-image-ubuntu'? I could not find any discription from NXP.

Sincerely


Gerry

0 项奖励
回复

757 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Since it not from NXP, But the BSP for Auto included drivers like CAN that are not in the ubuntu image, the ubuntu image just include the GUI and network.

Regards

 

0 项奖励
回复

683 次查看
Gerry15
Contributor III

Hey,

 

thank you for the answer. Unfortunately I am still not able to find out the login credentials for the `s32g274ardb2ubuntu` image.

As already discussed here Solved: login username and password failure - NXP Community, I have the right MACHINE activated, which is the s32g274ardb2ubuntu. "root root" does not work.

Do you have the login credentials documented somewhere?

 

Kind regards

 

Gerry

0 项奖励
回复