IPCF of S32G2 not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPCF of S32G2 not working

Jump to solution
1,277 Views

Hello,

I try the exemple IPCF_Example_S32G274 from package IPCF_4.3.0_D2109. When I build the project I have this error: ../src/sample.c:14:10: fatal error: ipcf_Ip_Cfg.h: No such file or directory

In the file where it is installed the IPCF driver, the file exist. I think the program don t see the file.

Best regards.

 

0 Kudos
Reply
1 Solution
1,272 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vlad,

Open the project default hardware/*.mex, then "Update code" could build all successfully..

 

Regards

View solution in original post

0 Kudos
Reply
2 Replies
1,273 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vlad,

Open the project default hardware/*.mex, then "Update code" could build all successfully..

 

Regards

0 Kudos
Reply
1,066 Views
shanlan123
Contributor II

I have done it, but still have this error: ../src/sample.c:14:10: fatal error: ipcf_Ip_Cfg.h: No such file or directory, please help me to solve this problem!

0 Kudos
Reply