Hi , there:
I'm Using S32G_SAF_2.0.0_EVAL packages to do an experiment, But I Don't know how to build the S32_SAF_Demo And Tresos project within the folder:
1. When i modified the launch.bat according my local environment ,and then executed it, then a error occured " ./Tresos/S32_SAF_S32G2XX_S32G274A/output/generated/src/Bist_Cfg.c:57:10: fatal error: S32_SAF_Version.h: No such file or directory "
2. when i use EB Tresos 27.1.0 import the eb project , most of the module has errors and can not execute genreate ,how can I resolve the problems?
can anyone help me ? thanks very much !!