I have flashed the SJA1110 firmware , but not able to share the internet from GMAC0 port to other devices connected to ethernet ports on S32G . Tried to enable SJA1110 on S32G with default sja1110_switch.bin from Goldvip 1.5.0 .
Also followed ethernet enablement guide from NXP Website to enable sja1110 switch . (Screenshot attached ) . But not able to get the IP for the PC connected to goldbox .
Please find the below logs
[ 4.766549] sja1110 spi5.1: Successfully configured!
[ 4.766600] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[ 4.782953] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'
[ 4.782972] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 320312
[ 4.783115] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid
[ 4.783190] sja1110 spi5.0: [sja1110_pre_uc_upload] µC not ready for download (Status=0x31)
[ 4.783471] sja1110 spi5.0: Uploading firmware...
[ 5.912053] sja1110 spi5.0: Upload successfully verified!
[ 5.938436] pfeng 46000000.pfe pfe0: configuring for fixed/sgmii link mode
[ 5.938791] pfeng 46000000.pfe pfe0: Link is Up - 1Gbps/Full - flow control off
[ 6.012975] pfeng 46000000.pfe: HIF1 started
[ 6.015651] pfeng 46000000.pfe pfe1: PHY [stmmac-0:08] driver [Aquantia AQR113c] (irq=POLL)
[ 6.015673] pfeng 46000000.pfe pfe1: configuring for phy/sgmii link mode
[ 6.015705] phy-s32gen1-serdes 44180000.serdes: Speed not supported
[ 6.099616] pfeng 46000000.pfe: HIF2 started
[ 6.164600] pfeng 46000000.pfe pfe2: PHY [PFEng Ethernet MDIO.2:04] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[ 6.164622] pfeng 46000000.pfe pfe2: configuring for phy/rgmii-id link mode