How to set pfe_mac2 to work in sgmii mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set pfe_mac2 to work in sgmii mode

1,267 Views
RiverHsieh
Contributor I

Questions:

1. I want to set pfe_mac2 to work in sgmii mode, but the uboot pfe driver always sets rgmii mode, how to set it correctly.The error message, modified device tree and source code are as follows.

2. In the pfe initialization of the kernel, pfe_mac2 is correctly set in sgmii mode. Before this, uboot sets rgmii mode, will it affect the kernel work?

 

Platform Description

Hardware: customized platform reference from s32g274ardb2

bsp: bsp33

PFE Firmware: PFE-FW_S32G_1.3.0

 

Uboot error message:

Using external clock for PCIe0, CRNS
Frequency 100Mhz configured for PCIe0
Configuring PCIe0 as RootComplex(x1)&SGMII [XPCS0 OFF(PCIex1), XPCS1 1G]
Using external clock for PCIe1, CRNS
Frequency 100Mhz configured for PCIe1

eth0: eth_eqosFailed to set the frequency of mac2_rx_rgmii
Failed to enable mac2_rx_rgmii clock
PFE: emac0: sgmii emac1: none emac2: rgmii

Warning: eth_pfeng using MAC address from ROM
, eth1: eth_pfeng
Hit any key to stop autoboot: 2 ### 1 ### 0
PFE: emac0: sgmii emac1: none emac2: rgmii
Failed to set the frequency of mac2_rx_rgmii

Uboot modify:


config S32GEN1_HWCONFIG
- default "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5" if (PCIE_S32GEN1 && FSL_PFENG) && NXP_S32GRDB_BOARD
+ default "pcie0:mode=rc&sgmii,clock=ext,fmhz=100,xpcs_mode=1;pcie1:mode=rc&sgmii,clock=ext,fmhz=100,xpcs_mode=0" if (PCIE_S32GEN1 && FSL_PFENG) && NXP_S32GRDB_BOARD

#if CONFIG_IS_ENABLED(NXP_S32GRDB_BOARD)
PHY_INTERFACE_MODE_SGMII, /* SJA1110A */
PHY_INTERFACE_MODE_SGMII, /* ARQ107/ARQ113 */
- PHY_INTERFACE_MODE_RGMII /* KSZ9031 */
+ PHY_INTERFACE_MODE_SGMII /* */

#ifdef CONFIG_FSL_PFENG
# define PFENG_EMAC "0"
-# define PFENG_MODE "enable,sgmii,none,rgmii"
+# define PFENG_MODE "enable,sgmii,none,sgmii"

kernel device tree modify:

&pfe_netif2 {
- phy-mode = "rgmii-id";
+ phy-mode = "sgmii";

kernel set sgmii message:

[ 3.220296] pfeng 46000000.pfe: Interface selected: EMAC0: 0x4 EMAC1: 0xffffffff EMAC2: 0x4
[ 3.220999] pfeng 46000000.pfe: PFE controller reset done
[ 3.221045] pfeng 46000000.pfe: TX clock on EMAC0 for interface sgmii installed
[ 3.221108] pfeng 46000000.pfe: RX clock on EMAC0 for interface sgmii installed
[ 3.221140] pfeng 46000000.pfe: TX clock on EMAC2 for interface sgmii installed
[ 3.221165] pfeng 46000000.pfe: RX clock on EMAC2 for interface sgmii installed

Tags (1)
0 Kudos
Reply
4 Replies

1,040 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @RiverHsieh,

Can we close this ticket?

 

Thanks,

Mayank s Patel

0 Kudos
Reply

1,034 Views
RiverHsieh
Contributor I

Yes,can be closed

Thanks,
River

0 Kudos
Reply

1,087 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @RiverHsieh,

Thank you for reaching out to us.

Can you please share the value of hwconfig variable from the u-boot console?

Use the below command to print the variable:

printenv hwconfig

 

0 Kudos
Reply

1,056 Views
RiverHsieh
Contributor I

Hi @MayanksPatel 

The problem has been solved, because when U-boot compiled the target board, the wrong PFENG_MODE was defined

Thanks

River

0 Kudos
Reply