How to run differentiated apps on different m7 cores ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run differentiated apps on different m7 cores ?

2,430件の閲覧回数
fengxianeric
Contributor IV

I am wondering whether we can run different apps on different m7 cores by start m7 command ?  If yes, how to do that ? Thanks

0 件の賞賛
返信
6 返答(返信)

2,410件の閲覧回数
SSyb
Contributor III

Depends on what an "app" is for you, You may want to try with a multicore-enabled operating system (like AUTOSAR-OS). Or bare metal: you can boot from flash different binaries on different cores, with the help of the NXP example bootloader for the M7. It is described in application note AN13750. If you want to omit the Linux part: also fine. you can choose to boot only the M7 cores with the bootloader too.

0 件の賞賛
返信

2,407件の閲覧回数
fengxianeric
Contributor IV

Thanks caring.

Let me talk with you about baremetal images firstly, and could you please tell me how to give address to startm7 command for different apps located in flash partition ?

Thanks

 

0 件の賞賛
返信

2,403件の閲覧回数
SSyb
Contributor III

Not sure what you mean with the "startm7 command" (but mayber that is because you did not explain the context...)

 

Anyway: when you use the bootloader, you configure which image to be started on which core in the EB Tresos tool. It is described in AN13750.

SSyb_0-1687250629268.png

 

What the generated bootloader source code internally does is to use the MC_ME engine of the S32G2 to prepare start addresses for the respective image fragments and then release the cores from reset. you don' t need to do this yourself if you use the bootloader.If you donÄt want to use a bootloader like this, you have to implement the logic yourself.

0 件の賞賛
返信

2,391件の閲覧回数
fengxianeric
Contributor IV

Thanks caring.

Not sure what you mean with the "startm7 command" (but mayber that is because you did not explain the context...)

[Eric] startm7 is the unique command for m7core under uboot as ipcf sample running method. We are considering the demo by such kind of command to run.

Thanks

 

0 件の賞賛
返信

2,386件の閲覧回数
SSyb
Contributor III

ah, ok. I was missign that part. UBOOT I have not used, and the bootloader I mentioned comes into play if it is the first thing you boot from the flash (or SD card).

If you want to use U-Boot, I guess my hint does not help.

0 件の賞賛
返信

2,383件の閲覧回数
fengxianeric
Contributor IV
Got your idea, keep in touch.
0 件の賞賛
返信