Hi Chenyin,
Thankyou for your quick reply.
I tried both the suggestion from you , here with the on board results which fails to boot further.
Suggestion 1: I tried loading LinuxVmwithRamDisk.uimage to 0x90000000.
LinuxVmwithRamDisk.uimage is an image build by integrating the ramdisk image (fsl-image-base-s32g399ardb3-20250317110053.rootfs.cpio.gz.u-boot).
Here with the test output on RDB3 board:
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
U-Boot 2022.04+g5a6f62071f+p0 (Sep 06 2024 - 07:11:20 +0000)
SoC: NXP S32G399A rev. 1.0
CPU: ARM Cortex-A53 r0p4 @ max 1300 MHz
Model: NXP S32G399A-RDB3
DRAM: 3.5 GiB
Core: 306 devices, 25 uclasses, devicetree: board
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
s32cc_serdes_phy serdes@40480000: Using mode 0 for SerDes subsystem
pci_s32cc pcie@40400000: Configuring as RootComplex
pci_s32cc pcie@40400000: Failed to get link up
In: serial@401c8000
Out: serial@401c8000
Err: serial@401c8000
Board revision: RDB3 Revision E
PCIe: BusDevFun VendorId DeviceId Device Class Sub-Class
__________________________________________________________________________
pcie@40400000 RootComplex
| `-- 01:00.00 0x1957 0x4300 Bridge device 0x04
Net:
Warning: ethernet@4033c000 (eth0) using random MAC address - a6:61:3e:2c:fe:af
eth0: ethernet@4033c000
Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2
Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2
Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2
Hit any key to stop autoboot: 0
=>
=>
=> fatload mmc 0:1 0x85000000 s32g399a-rdb3.dtb
60416 bytes read in 7 ms (8.2 MiB/s)
=> ext4load mmc 0:2 0x90000000 /home/root/LinuxVmwithRamDisk.uimage
154534148 bytes read in 6414 ms (23 MiB/s)
=> bootm 0x90000000 - 0x85000000
## Booting kernel from Legacy Image at 90000000 ...
Image Name: L4 Image #15
Image Type: AArch64 Linux Kernel Image (uncompressed)
Data Size: 154534084 Bytes = 147.4 MiB
Load Address: 81200000
Entry Point: 81200000
Verifying Checksum ... OK
## Flattened Device Tree blob at 85000000
Booting using the fdt blob at 0x85000000
Loading Kernel Image
uncompressed: uncompress error -28
Must RESET board to recover
bootm - boot application image from memory
Usage:
bootm [addr [arg ...]]
- boot application image stored in memory
passing arguments 'arg ...'; when booting a Linux kernel,
'arg' can be the address of an initrd image
When booting a Linux kernel which requires a flat device-tree
a third argument is required which is the address of the
device-tree blob. To boot that kernel without an initrd image,
use a '-' for the second argument. If you do not pass a third
a bd_info struct will be passed instead
Sub-commands to do part of the bootm sequence. The sub-commands must be
issued in the order below (it's ok to not issue all sub-commands):
start [addr [arg ...]]
loados - load OS image
ramdisk - relocate initrd, set env initrd_start/initrd_end
fdt - relocate flat device tree
cmdline - OS specific command line processing/setup
bdt - OS specific bd_info processing
prep - OS specific prep before relocation or go
go - start OS
=>
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Suggestion 2: I tied the smaller RAM disk image generated from "bitbake core-image-minimal" (Imgae Output -core-image-minimal-s32g399ardb3-20250325052917.rootfs.cpio.gz.u-boot)
It gives kernel panic "Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)"as below board logs:
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
MOE: Starting: rom/ned rom/linux-vm.cfg
MOE: loading 'rom/ned'
Ned says: Hi World!
Ned: loading file: 'rom/linux-vm.cfg'
Console Server
cons>
Created vcon channel: switch [420010]
cons>
switch | Max number of buffers in virtqueue: 256
Created vcon channel: vm1 [421010]
cons>
Created vcon channel: mon1 [422010]
cons>
vm1 | VMM[main]: Hello out there.
Created vcon channel: vm2 [423010]
cons>
Created vcon channel: mon2 [424010]
cons>
vm2 | VMM[main]: Hello out there.
switch | Registering dataspace from 0x90200000 with 131072 KiB, offset 0x0
switch | PORT[0x14d70]: DMA guest [90200000-981fffff] local [1200000-91fffff] offset 0
switch | register client: host IRQ: 420010 config DS: 41d000
vm1 | VMM[ram]: Cleaning caches for device tree [9fff000-9fff9ac] ([981ff000])
vm1 | VMM: Hello clock source for vCPU 0
switch | Registering dataspace from 0x98200000 with 131072 KiB, offset 0x0
vm1 | VMM: Hello clock source for vCPU 1
switch | PORT[0x14e80]: DMA guest [98200000-a01fffff] local [9200000-111fffff] offset 0
switch | register client: host IRQ: 420010 config DS: 41e000
vm1 | VMM: Hello clock source for vCPU 2
vm2 | VMM[ram]: Cleaning caches for device tree [9fff000-9fff9ac] ([a01ff000])
vm1 | VMM: Hello clock source for vCPU 3
vm2 | VMM: Hello clock source for vCPU 0
vm2 | VMM: Hello clock source for vCPU 1
vm1 | VMM: Starting Cpu0 @ 0x90200000 in 64Bit mode (handler @ 109c61c, stack: 801ffc10, task: 41e000, mpidr: 80000000 (orig: 80000000)
vm2 | VMM: Hello clock source for vCPU 2
vm1 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm2 | VMM: Hello clock source for vCPU 3
vm2 | VMM: Starting Cpu0 @ 0x98200000 in 64Bit mode (handler @ 109c61c, stack: 801ffc10, task: 41e000, mpidr: 80000000 (orig: 80000000)
vm2 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm1 | VMM: Starting Cpu1 @ 0x90eb2338 in 64Bit mode (handler @ 109c61c, stack: 430f30, task: 41e000, mpidr: 80000001 (orig: 80000000)
vm1 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm1 | VMM: Starting Cpu2 @ 0x90eb2338 in 64Bit mode (handler @ 109c61c, stack: 82ff30, task: 41e000, mpidr: 80000002 (orig: 80000000)
vm1 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm1 | VMM: Starting Cpu3 @ 0x90eb2338 in 64Bit mode (handler @ 109c61c, stack: c2ff30, task: 41e000, mpidr: 80000003 (orig: 80000000)
vm1 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm1 | [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
vm1 | [ 0.000000] Linux version 6.6.32-rt32-g49d9f8bb25e0 (gvt1kor@BANI-C-007L8) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.2) 9.4.0, GNU ld (GNU Binutils for Ubuntu) 2.34) #2 SMP PREEMPT Fri Mar 21 16:38:57 IST 2025
vm1 | [ 0.000000] Zone ranges:
vm1 | [ 0.000000] DMA [mem 0x0000000090200000-0x00000000981fffff]
vm2 | VMM: Starting Cpu1 @ 0x98eb2338 in 64Bit mode (handler @ 109c61c, stack: 430f30, task: 41e000, mpidr: 80000001 (orig: 80000000)
vm2 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm2 | VMM: Starting Cpu2 @ 0x98eb2338 in 64Bit mode (handler @ 109c61c, stack: 82ff30, task: 41e000, mpidr: 80000002 (orig: 80000000)
vm2 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm2 | VMM: Starting Cpu3 @ 0x98eb2338 in 64Bit mode (handler @ 109c61c, stack: c2ff30, task: 41e000, mpidr: 80000003 (orig: 80000000)
vm2 | VMM: FATAL: ffffffc08002160c: mrs r0, S3_1_C11_C0_2 (hsr=62346c01)
vm1 | [ 0.000000] DMA32 empty
vm1 | [ 0.000000] Normal empty
vm1 | [ 0.000000] Movable zone start for each node
vm2 | [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
vm1 | [ 0.000000] Early memory node ranges
vm1 | [ 0.000000] node 0: [mem 0x0000000090200000-0x00000000981fffff]
vm1 | [ 0.000000] Initmem setup node 0 [mem 0x0000000090200000-0x00000000981fffff]
vm2 | [ 0.000000] Linux version 6.6.32-rt32-g49d9f8bb25e0 (gvt1kor@BANI-C-007L8) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.2) 9.4.0, GNU ld (GNU Binutils for Ubuntu) 2.34) #2 SMP PREEMPT Fri Mar 21 16:38:57 IST 2025
vm1 | [ 0.000000] On node 0, zone DMA: 512 pages in unavailable ranges
vm2 | [ 0.000000] Zone ranges:
vm1 | [ 0.000000] On node 0, zone DMA: 32256 pages in unavailable ranges
vm2 | [ 0.000000] DMA [mem 0x0000000098200000-0x00000000a01fffff]
vm1 | [ 0.000000] cma: Failed to reserve 256 MiB on node -1
vm2 | [ 0.000000] DMA32 empty
vm2 | [ 0.000000] Normal empty
vm1 | [ 0.000000] psci: probing for conduit method from DT.
vm2 | [ 0.000000] Movable zone start for each node
vm1 | [ 0.000000] psci: PSCIv1.0 detected in firmware.
vm2 | [ 0.000000] Early memory node ranges
vm1 | [ 0.000000] psci: Using standard PSCI v0.2 function IDs
vm2 | [ 0.000000] node 0: [mem 0x0000000098200000-0x00000000a01fffff]
vm1 | [ 0.000000] psci: Trusted OS migration not required
vm1 | [ 0.000000] psci: SMC Calling Convention v1.0
vm2 | [ 0.000000] Initmem setup node 0 [mem 0x0000000098200000-0x00000000a01fffff]
vm1 | [ 0.000000] percpu: Embedded 20 pages/cpu s44840 r8192 d28888 u81920
vm2 | [ 0.000000] On node 0, zone DMA: 512 pages in unavailable ranges
vm1 | [ 0.000000] Detected VIPT I-cache on CPU0
vm2 | [ 0.000000] On node 0, zone DMA: 32256 pages in unavailable ranges
vm1 | [ 0.000000] CPU features: detected: GIC system register CPU interface
vm2 | [ 0.000000] cma: Failed to reserve 256 MiB on node -1
vm1 | [ 0.000000] CPU features: detected: ARM erratum 845719
vm2 | [ 0.000000] psci: probing for conduit method from DT.
vm2 | [ 0.000000] psci: PSCIv1.0 detected in firmware.
vm1 | [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, 1530923, or 1530924
vm2 | [ 0.000000] psci: Using standard PSCI v0.2 function IDs
vm1 | [ 0.000000] alternatives: applying boot alternatives
vm2 | [ 0.000000] psci: Trusted OS migration not required
vm2 | [ 0.000000] psci: SMC Calling Convention v1.0
vm1 | [ 0.000000] Kernel command line: console=ttyAMA0 earlyprintk=1 rdinit=/init ip=192.168.1.1:::255.255.255.0:server:eth0
vm2 | [ 0.000000] percpu: Embedded 20 pages/cpu s44840 r8192 d28888 u81920
vm2 | [ 0.000000] Detected VIPT I-cache on CPU0
vm1 | [ 0.000000] Unknown kernel command line parameters "earlyprintk=1", will be passed to user space.
vm2 | [ 0.000000] CPU features: detected: GIC system register CPU interface
vm1 | [ 0.000000] Dentry cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
vm2 | [ 0.000000] CPU features: detected: ARM erratum 845719
vm1 | [ 0.000000] Inode-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
vm2 | [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, 1530923, or 1530924
vm1 | [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 32256
vm2 | [ 0.000000] alternatives: applying boot alternatives
vm1 | [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
vm1 | [ 0.000000] software IO TLB: area num 4.
vm2 | [ 0.000000] Kernel command line: console=ttyAMA0 earlyprintk=1 rdinit=/init ip=192.168.1.2:::255.255.255.0:server:eth0
vm1 | [ 0.000000] software IO TLB: mapped [mem 0x0000000092e00000-0x0000000096e00000] (64MB)
vm2 | [ 0.000000] Unknown kernel command line parameters "earlyprintk=1", will be passed to user space.
vm2 | [ 0.000000] Dentry cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
vm1 | [ 0.000000] Memory: 29500K/131072K available (9792K kernel code, 662K rwdata, 3112K rodata, 1920K init, 226K bss, 101572K reserved, 0K cma-reserved)
vm2 | [ 0.000000] Inode-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
vm1 | [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
vm2 | [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 32256
vm1 | [ 0.000000] rcu: Preemptible hierarchical RCU implementation.
vm1 | [ 0.000000] rcu: RCU event tracing is enabled.
vm2 | [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
vm2 | [ 0.000000] software IO TLB: area num 4.
vm1 | [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
vm1 | [ 0.000000] Trampoline variant of Tasks RCU enabled.
vm2 | [ 0.000000] software IO TLB: mapped [mem 0x000000009ae00000-0x000000009ee00000] (64MB)
vm1 | [ 0.000000] Tracing variant of Tasks RCU enabled.
vm1 | [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
vm2 | [ 0.000000] Memory: 29500K/131072K available (9792K kernel code, 662K rwdata, 3112K rodata, 1920K init, 226K bss, 101572K reserved, 0K cma-reserved)
vm1 | [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
vm2 | [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
vm1 | [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
vm2 | [ 0.000000] rcu: Preemptible hierarchical RCU implementation.
vm1 | [ 0.000000] GICv3: 988 SPIs implemented
vm2 | [ 0.000000] rcu: RCU event tracing is enabled.
vm1 | [ 0.000000] GICv3: 0 Extended SPIs implemented
vm1 | [ 0.000000] Root IRQ handler: gic_handle_irq
vm2 | [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
vm1 | [ 0.000000] GICv3: GICv3 features: 16 PPIs
vm2 | [ 0.000000] Trampoline variant of Tasks RCU enabled.
vm2 | [ 0.000000] Tracing variant of Tasks RCU enabled.
vm1 | [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000000050000
vm1 | [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
vm2 | [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
vm1 | [ 0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (virt).
vm2 | [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
vm2 | [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
vm2 | [ 0.000000] GICv3: 988 SPIs implemented
vm1 | [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
vm2 | [ 0.000000] GICv3: 0 Extended SPIs implemented
vm1 | [ 0.000001] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
vm2 | [ 0.000000] Root IRQ handler: gic_handle_irq
vm1 | [ 0.000161] Console: colour dummy device 80x25
vm2 | [ 0.000000] GICv3: GICv3 features: 16 PPIs
vm2 | [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000000050000
vm1 | [ 0.000190] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
vm2 | [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
vm1 | [ 0.000201] pid_max: default: 32768 minimum: 301
vm2 | [ 0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (virt).
vm1 | [ 0.000296] Mount-cache hash table entries: 512 (order: 0, 4096 bytes, linear)
vm1 | [ 0.000306] Mountpoint-cache hash table entries: 512 (order: 0, 4096 bytes, linear)
vm2 | [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
vm1 | [ 0.001012] cacheinfo: Unable to detect cache hierarchy for CPU 0
vm2 | [ 0.000000] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
vm1 | [ 0.001846] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
vm2 | [ 0.000165] Console: colour dummy device 80x25
vm1 | [ 0.001937] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
vm2 | [ 0.000196] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
vm1 | [ 0.002128] rcu: Hierarchical SRCU implementation.
vm2 | [ 0.000207] pid_max: default: 32768 minimum: 301
vm1 | [ 0.002132] rcu: Max phase no-delay instances is 1000.
vm1 | [ 0.002571] smp: Bringing up secondary CPUs ...
vm2 | [ 0.000304] Mount-cache hash table entries: 512 (order: 0, 4096 bytes, linear)
vm1 | [ 0.016501] Detected VIPT I-cache on CPU1
vm2 | [ 0.000313] Mountpoint-cache hash table entries: 512 (order: 0, 4096 bytes, linear)
vm1 | [ 0.016561] GICv3: CPU1: found redistributor 1 region 0:0x0000000000070000
vm2 | [ 0.001036] cacheinfo: Unable to detect cache hierarchy for CPU 0
vm1 | [ 0.016662] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
vm2 | [ 0.001877] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
vm1 | [ 0.038083] Detected VIPT I-cache on CPU2
vm1 | [ 0.038126] GICv3: CPU2: found redistributor 2 region 0:0x0000000000090000
vm2 | [ 0.001961] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
vm2 | [ 0.002157] rcu: Hierarchical SRCU implementation.
vm1 | [ 0.038210] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
vm2 | [ 0.002160] rcu: Max phase no-delay instances is 1000.
vm1 | [ 0.059603] Detected VIPT I-cache on CPU3
vm2 | [ 0.002610] smp: Bringing up secondary CPUs ...
vm1 | [ 0.059649] GICv3: CPU3: found redistributor 3 region 0:0x00000000000b0000
vm2 | [ 0.016679] Detected VIPT I-cache on CPU1
vm1 | [ 0.059732] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
vm2 | [ 0.016739] GICv3: CPU1: found redistributor 1 region 0:0x0000000000070000
vm1 | [ 0.067390] smp: Brought up 1 node, 4 CPUs
vm2 | [ 0.016844] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
vm1 | [ 0.067397] SMP: Total of 4 processors activated.
vm2 | [ 0.038280] Detected VIPT I-cache on CPU2
vm1 | [ 0.067401] CPU features: detected: 32-bit EL0 Support
vm2 | [ 0.038324] GICv3: CPU2: found redistributor 2 region 0:0x0000000000090000
vm1 | [ 0.067403] CPU features: detected: 32-bit EL1 Support
vm1 | [ 0.067408] CPU features: detected: CRC32 instructions
vm2 | [ 0.038407] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
vm1 | [ 0.067494] CPU: All CPU(s) started at EL1
vm2 | [ 0.059835] Detected VIPT I-cache on CPU3
vm1 | [ 0.067507] alternatives: applying system-wide alternatives
vm2 | [ 0.059885] GICv3: CPU3: found redistributor 3 region 0:0x00000000000b0000
vm1 | [ 0.068940] devtmpfs: initialized
vm2 | [ 0.059967] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
vm1 | [ 0.069946] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
vm2 | [ 0.067622] smp: Brought up 1 node, 4 CPUs
vm2 | [ 0.067629] SMP: Total of 4 processors activated.
vm1 | [ 0.069961] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
vm2 | [ 0.067633] CPU features: detected: 32-bit EL0 Support
vm1 | [ 0.070085] pinctrl core: initialized pinctrl subsystem
vm2 | [ 0.067636] CPU features: detected: 32-bit EL1 Support
vm1 | [ 0.070780] NET: Registered PF_NETLINK/PF_ROUTE protocol family
vm2 | [ 0.067641] CPU features: detected: CRC32 instructions
vm2 | [ 0.067728] CPU: All CPU(s) started at EL1
vm1 | [ 0.071235] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
vm2 | [ 0.067741] alternatives: applying system-wide alternatives
vm1 | [ 0.071275] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
vm2 | [ 0.073982] devtmpfs: initialized
vm1 | [ 0.071310] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
vm2 | [ 0.075001] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
vm1 | [ 0.071637] thermal_sys: Registered thermal governor 'step_wise'
vm2 | [ 0.075016] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
vm1 | [ 0.071723] hw-breakpoint: found 1 breakpoint and 1 watchpoint registers.
vm2 | [ 0.075144] pinctrl core: initialized pinctrl subsystem
vm1 | [ 0.071899] ASID allocator initialised with 65536 entries
vm2 | [ 0.075843] NET: Registered PF_NETLINK/PF_ROUTE protocol family
vm1 | [ 0.072012] Serial: AMBA PL011 UART driver
vm1 | [ 0.072055] scmi_core: SCMI protocol bus registered
vm2 | [ 0.076307] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
vm2 | [ 0.076344] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
vm1 | [ 0.072785] 12000.pl011_uart: ttyAMA0 at MMIO 0x12000 (irq = 13, base_baud = 0) is a PL011 rev3
vm1 | [ 0.072828] printk: legacy console [ttyAMA0] enabled
vm2 | [ 0.076379] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
vm1 | [ 1.696561] Modules: 28784 pages in range for non-PLT usage
vm2 | [ 0.076686] thermal_sys: Registered thermal governor 'step_wise'
vm1 | [ 1.696576] Modules: 520304 pages in range for PLT usage
vm2 | [ 0.076772] hw-breakpoint: found 1 breakpoint and 1 watchpoint registers.
vm1 | [ 1.715291] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
vm2 | [ 0.076925] ASID allocator initialised with 65536 entries
vm2 | [ 0.077032] Serial: AMBA PL011 UART driver
vm1 | [ 1.741033] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
vm2 | [ 0.077075] scmi_core: SCMI protocol bus registered
vm1 | [ 1.764009] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
vm2 | [ 0.077829] 12000.pl011_uart: ttyAMA0 at MMIO 0x12000 (irq = 13, base_baud = 0) is a PL011 rev3
vm1 | [ 1.780003] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
vm2 | [ 0.077872] printk: legacy console [ttyAMA0] enabled
vm1 | [ 1.800365] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
vm2 | [ 1.667857] Modules: 28784 pages in range for non-PLT usage
vm1 | [ 1.817431] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
vm2 | [ 1.667871] Modules: 520304 pages in range for PLT usage
vm1 | [ 1.834847] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
vm2 | [ 1.685428] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
vm1 | [ 1.851292] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
vm2 | [ 1.711459] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
vm1 | [ 1.878557] SCSI subsystem initialized
vm1 | [ 1.887571] usbcore: registered new interface driver usbfs
vm2 | [ 1.730046] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
vm1 | [ 1.894087] usbcore: registered new interface driver hub
vm2 | [ 1.752556] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
vm1 | [ 1.911076] usbcore: registered new device driver usb
vm2 | [ 1.769502] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
vm1 | [ 1.927420] pps_core: LinuxPPS API ver. 1 registered
vm2 | [ 1.785830] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
vm1 | [ 1.943874] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
vm2 | [ 1.802383] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
vm1 | [ 1.960319] PTP clock support registered
vm1 | [ 1.987492] vgaarb: loaded
vm2 | [ 1.822755] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
vm1 | [ 1.992727] clocksource: Switched to clocksource arch_sys_counter
vm2 | [ 1.852877] SCSI subsystem initialized
vm2 | [ 1.862232] usbcore: registered new interface driver usbfs
vm2 | [ 1.869753] usbcore: registered new interface driver hub
vm2 | [ 1.879114] usbcore: registered new device driver usb
vm2 | [ 1.888270] pps_core: LinuxPPS API ver. 1 registered
vm1 | [ 2.046400] NET: Registered PF_INET protocol family
vm2 | [ 1.897132] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
vm1 | [ 2.054162] IP idents hash table entries: 2048 (order: 2, 16384 bytes, linear)
vm2 | [ 1.912455] PTP clock support registered
vm2 | [ 1.940619] vgaarb: loaded
vm1 | [ 2.073588] tcp_listen_portaddr_hash hash table entries: 256 (order: 0, 4096 bytes, linear)
vm2 | [ 1.945869] clocksource: Switched to clocksource arch_sys_counter
vm1 | [ 2.095864] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
vm1 | [ 2.116971] TCP established hash table entries: 1024 (order: 1, 8192 bytes, linear)
vm1 | [ 2.129372] TCP bind hash table entries: 1024 (order: 3, 32768 bytes, linear)
vm2 | [ 1.992768] NET: Registered PF_INET protocol family
vm1 | [ 2.141581] TCP: Hash tables configured (established 1024 bind 1024)
vm2 | [ 2.002732] IP idents hash table entries: 2048 (order: 2, 16384 bytes, linear)
vm1 | [ 2.159004] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
vm1 | [ 2.177925] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
vm2 | [ 2.019429] tcp_listen_portaddr_hash hash table entries: 256 (order: 0, 4096 bytes, linear)
vm1 | [ 2.187625] NET: Registered PF_UNIX/PF_LOCAL protocol family
vm2 | [ 2.047590] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
vm1 | [ 2.215806] RPC: Registered named UNIX socket transport module.
vm2 | [ 2.066970] TCP established hash table entries: 1024 (order: 1, 8192 bytes, linear)
vm1 | [ 2.226485] RPC: Registered udp transport module.
vm1 | [ 2.244724] RPC: Registered tcp transport module.
vm2 | [ 2.085722] TCP bind hash table entries: 1024 (order: 3, 32768 bytes, linear)
vm1 | [ 2.252035] RPC: Registered tcp-with-tls transport module.
vm2 | [ 2.109700] TCP: Hash tables configured (established 1024 bind 1024)
vm1 | [ 2.268592] RPC: Registered tcp NFSv4.1 backchannel transport module.
vm2 | [ 2.127253] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
vm1 | [ 2.285379] PCI: CLS 0 bytes, default 64
vm2 | [ 2.144951] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
vm1 | [ 2.303167] kvm [1]: HYP mode not available
vm1 | [ 2.309052] Unpacking initramfs...
vm2 | [ 2.168122] NET: Registered PF_UNIX/PF_LOCAL protocol family
vm1 | [ 2.327140] workingset: timestamp_bits=62 max_order=13 bucket_order=0
vm2 | [ 2.197295] RPC: Registered named UNIX socket transport module.
vm1 | [ 2.327707] fuse: init (API version 7.39)
vm2 | [ 2.206651] RPC: Registered udp transport module.
vm1 | [ 2.327878] NET: Registered PF_ALG protocol family
vm2 | [ 2.221136] RPC: Registered tcp transport module.
vm2 | [ 2.235155] RPC: Registered tcp-with-tls transport module.
vm1 | [ 2.327924] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
vm1 | [ 2.327934] io scheduler mq-deadline registered
vm2 | [ 2.242581] RPC: Registered tcp NFSv4.1 backchannel transport module.
vm1 | [ 2.327939] io scheduler kyber registered
vm2 | [ 2.266767] PCI: CLS 0 bytes, default 64
vm1 | [ 2.327951] io scheduler bfq registered
vm2 | [ 2.282119] Unpacking initramfs...
vm1 | [ 2.437143] Initramfs unpacking failed: invalid magic at start of compressed archive
switch | Resetting device
vm2 | [ 2.294248] Initramfs unpacking failed: invalid magic at start of compressed archive
vm1 | [ 2.462934] Freeing initrd memory: 14424K
vm1 | [ 2.484454] vcan: Virtual CAN interface driver
vm2 | [ 2.299535] kvm [1]: HYP mode not available
vm1 | [ 2.487972] slcan: serial line CAN interface driver
vm2 | [ 2.327859] Freeing initrd memory: 14424K
vm1 | [ 2.500839] CAN device driver interface
vm2 | [ 2.365315] workingset: timestamp_bits=62 max_order=14 bucket_order=0
vm1 | [ 2.514908] e100: Intel(R) PRO/100 Network Driver
vm2 | [ 2.387491] fuse: init (API version 7.39)
vm1 | [ 2.530027] e100: Copyright(c) 1999-2006 Intel Corporation
vm2 | [ 2.401561] NET: Registered PF_ALG protocol family
vm1 | [ 2.543291] e1000: Intel(R) PRO/1000 Network Driver
vm2 | [ 2.408867] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
vm1 | [ 2.558056] e1000: Copyright (c) 1999-2006 Intel Corporation.
vm2 | [ 2.416331] io scheduler mq-deadline registered
vm1 | [ 2.575110] e1000e: Intel(R) PRO/1000 Network Driver
vm2 | [ 2.433853] io scheduler kyber registered
vm2 | [ 2.447614] io scheduler bfq registered
vm1 | [ 2.589840] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
vm1 | [ 2.609292] igb: Intel(R) Gigabit Ethernet Network Driver
vm1 | [ 2.617612] igb: Copyright (c) 2007-2014 Intel Corporation.
switch | Resetting device
vm1 | [ 2.633332] usbcore: registered new interface driver uas
vm1 | [ 2.637854] usbcore: registered new interface driver usb-storage
vm1 | [ 2.654234] i2c_dev: i2c /dev entries driver
vm1 | [ 2.654824] sdhci: Secure Digital Host Controller Interface driver
vm1 | [ 2.661417] sdhci: Copyright(c) Pierre Ossman
vm1 | [ 2.670031] sdhci-pltfm: SDHCI platform and OF driver helper
vm1 | [ 2.677017] usbcore: registered new interface driver usbhid
vm1 | [ 2.685045] usbhid: USB HID core driver
vm1 | [ 2.693444] NET: Registered PF_INET6 protocol family
vm1 | [ 2.699985] Segment Routing with IPv6
vm2 | [ 2.558697] vcan: Virtual CAN interface driver
vm1 | [ 2.708392] In-situ OAM (IOAM) with IPv6
vm2 | [ 2.564731] slcan: serial line CAN interface driver
vm2 | [ 2.584126] CAN device driver interface
vm1 | [ 2.720646] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
vm2 | [ 2.590293] e100: Intel(R) PRO/100 Network Driver
vm2 | [ 2.598552] e100: Copyright(c) 1999-2006 Intel Corporation
vm1 | [ 2.740107] NET: Registered PF_PACKET protocol family
vm2 | [ 2.605653] e1000: Intel(R) PRO/1000 Network Driver
vm1 | [ 2.769354] can: controller area network core
vm2 | [ 2.620513] e1000: Copyright (c) 1999-2006 Intel Corporation.
vm2 | [ 2.634098] e1000e: Intel(R) PRO/1000 Network Driver
vm1 | [ 2.776771] NET: Registered PF_CAN protocol family
vm2 | [ 2.642193] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
vm1 | [ 2.798367] can: raw protocol
vm2 | [ 2.656297] igb: Intel(R) Gigabit Ethernet Network Driver
vm1 | [ 2.813444] can: broadcast manager protocol
vm2 | [ 2.669428] igb: Copyright (c) 2007-2014 Intel Corporation.
vm1 | [ 2.826277] can: netlink gateway - max_hops=1
vm1 | [ 2.840735] 8021q: 802.1Q VLAN Support v1.8
vm2 | [ 2.697784] usbcore: registered new interface driver uas
vm2 | [ 2.704536] usbcore: registered new interface driver usb-storage
vm2 | [ 2.720879] i2c_dev: i2c /dev entries driver
vm2 | [ 2.727569] sdhci: Secure Digital Host Controller Interface driver
vm2 | [ 2.736124] sdhci: Copyright(c) Pierre Ossman
vm2 | [ 2.742680] sdhci-pltfm: SDHCI platform and OF driver helper
vm2 | [ 2.750848] usbcore: registered new interface driver usbhid
vm2 | [ 2.758734] usbhid: USB HID core driver
vm2 | [ 2.765216] NET: Registered PF_INET6 protocol family
vm2 | [ 2.773306] Segment Routing with IPv6
vm2 | [ 2.779151] In-situ OAM (IOAM) with IPv6
vm2 | [ 2.785273] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
vm2 | [ 2.793970] NET: Registered PF_PACKET protocol family
vm2 | [ 2.801437] can: controller area network core
vm2 | [ 2.808037] NET: Registered PF_CAN protocol family
vm2 | [ 2.815068] can: raw protocol
vm2 | [ 2.820110] can: broadcast manager protocol
vm2 | [ 2.826478] can: netlink gateway - max_hops=1
vm2 | [ 2.833089] 8021q: 802.1Q VLAN Support v1.8
vm1 | [ 15.129526] clk: Disabling unused clocks
vm1 | [ 15.135764] uart-pl011 12000.pl011_uart: no DMA platform data
vm1 | [ 15.144547] /dev/root: Can't open blockdev
vm1 | [ 15.150925] VFS: Cannot open root device "" or unknown-block(0,0): error -6
vm1 | [ 15.160480] Please append a correct "root=" boot option; here are the available partitions:
vm1 | [ 15.171521] List of all bdev filesystems:
vm1 | [ 15.177770] ext3
vm1 | [ 15.177774] ext4
vm1 | [ 15.181698] ext2
vm1 | [ 15.185650] vfat
vm1 | [ 15.189573] fuseblk
vm1 | [ 15.193526]
vm1 | [ 15.201208] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
vm1 | [ 15.212139] SMP: stopping secondary CPUs
vm1 | [ 15.218298] Kernel Offset: disabled
vm1 | [ 15.228656] CPU features: 0x1,00000008,00020000,1000421b
vm1 | [ 15.236336] Memory Limit: none
vm1 | [ 15.251660] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---
vm2 | [ 15.142641] clk: Disabling unused clocks
vm2 | [ 15.149004] uart-pl011 12000.pl011_uart: no DMA platform data
vm2 | [ 15.161224] /dev/root: Can't open blockdev
vm2 | [ 15.167526] VFS: Cannot open root device "" or unknown-block(0,0): error -6
vm2 | [ 15.187528] Please append a correct "root=" boot option; here are the available partitions:
vm2 | [ 15.208540] List of all bdev filesystems:
vm2 | [ 15.214720] ext3
vm2 | [ 15.214725] ext4
vm2 | [ 15.218627] ext2
vm2 | [ 15.232534] vfat
vm2 | [ 15.236437] fuseblk
vm2 | [ 15.240341]
vm2 | [ 15.257965] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
vm2 | [ 15.279527] SMP: stopping secondary CPUs
vm2 | [ 15.285615] Kernel Offset: disabled
vm2 | [ 15.301527] CPU features: 0x1,00000008,00020000,1000421b
vm2 | [ 15.309122] Memory Limit: none
vm2 | [ 15.324530] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Regards,
Vishal