How could i generate Siul_Dio_Ip_Cfg.h in S32G-VNP-RDB2 RGB LED example?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How could i generate Siul_Dio_Ip_Cfg.h in S32G-VNP-RDB2 RGB LED example?

606 Views
davidNad
Contributor I

I'm having trouble proceeding with 'Light Up RGB LED Based On Real Time Drivers' 

I'm working on S32G-VNP-RDB2-SW-UG document.

After I 'Check Configuration and update code' (page 16), there is no Siul2_Dio_ip_Cfg.h.
(I do Pins configuration and add GPIO Drivers)

After that, if i follow the documentation as it is, it seems that the error occurs because that file(Cfg.h) does not exist.

I am working on Ubuntu 18.04 and S32 Design studio's version is 3.4. 

 

Could you let mo know how i can create/generate that configuration header file?

0 Kudos
Reply
1 Reply

582 Views
yonghwi_lee
NXP Employee
NXP Employee

Hello David Na,

1. Could you check "Siul2_Dio" driver is added correctly?

yonghwi_lee_1-1664932389723.png

2. Could you check Update Files as below and see if there is "Siul2_Dio_ip_Cfg.h"?

yonghwi_lee_0-1664932139576.png

Thanks,
Yonghwi Lee

0 Kudos
Reply