How can2eth and eth2can running on S32G A-core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can2eth and eth2can running on S32G A-core

ソリューションへジャンプ
155件の閲覧回数
GG0712
Contributor III

Hi NXP team,

 

I'm using s32g399ardb3 and BSP43 to test LLCE's can2can, can2eth, and eth2can features.

According to AN13423, the eth2can and can2eth examples are designed to run on M-core.

How can I use eth2can and can2eth on A-core without using M-core?

 

Thanks

0 件の賞賛
返信
1 解決策
127件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

From the software view, CAN2ETH and ETH2CAN are currently only implemented based on RTD/LLCE FW using on M cores, they are not currently implemented under Linux for A core BSP side.

Sorry for your inconvenience.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
128件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

From the software view, CAN2ETH and ETH2CAN are currently only implemented based on RTD/LLCE FW using on M cores, they are not currently implemented under Linux for A core BSP side.

Sorry for your inconvenience.

 

BR

Chenyin

0 件の賞賛
返信