How can2eth and eth2can running on S32G A-core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can2eth and eth2can running on S32G A-core

Jump to solution
148 Views
GG0712
Contributor III

Hi NXP team,

 

I'm using s32g399ardb3 and BSP43 to test LLCE's can2can, can2eth, and eth2can features.

According to AN13423, the eth2can and can2eth examples are designed to run on M-core.

How can I use eth2can and can2eth on A-core without using M-core?

 

Thanks

0 Kudos
Reply
1 Solution
120 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

From the software view, CAN2ETH and ETH2CAN are currently only implemented based on RTD/LLCE FW using on M cores, they are not currently implemented under Linux for A core BSP side.

Sorry for your inconvenience.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
1 Reply
121 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

From the software view, CAN2ETH and ETH2CAN are currently only implemented based on RTD/LLCE FW using on M cores, they are not currently implemented under Linux for A core BSP side.

Sorry for your inconvenience.

 

BR

Chenyin

0 Kudos
Reply