I'm assuming the board in question in S32G-VNP-RDB2, not S32G274ARDB, which is
an invalid part number. There is a document specific to your board which
describes exactly what you want - boot S32G2 M7 core from an SD card directly
into an application created in S32DS:
https://www.nxp.com/webapp/Download?colCode=S32G-VNP-RDB2-SW-UG
If you want to create a workable demo for an M7 SD card boot, all that you need
is to follow it strictly. The same slides discussing IVT, DCD and the linker file
give you the checkpoints for a modified code. If you changed the demo code and it
fails with with your modifications, you have to debug it. See S32DS User Guide,
section titled "Debugging with S32 Debug Probe from flash for all other targets"
on page 100.
Additional information on the bootable SD card image layout and SD card boot
flow can be found in S32G2RM, Sections 30.4 and 30.13.2
Best Regards,
Platon