Goldvip: how to compile fsl-image-goldvip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Goldvip: how to compile fsl-image-goldvip

Jump to solution
2,160 Views
fenghua_jiang
Contributor IV

Hello team,

      I follow some steps to compile image of goldvip,but it failed.

      step 1:

   $ mkdir ~/bin
   $ curl http://commondatastorage.googleapis.com/git-repo-downloads/
       repo > ~/bin/repo
   $ chmod a+x ~/bin/repo PATH=${PATH}:~/bin

      step 2:

$ mkdir nxp-yocto-goldvip
$ cd nxp-yocto-goldvip
$ repo init -u https://source.codeaurora.org/external/autobsps32/
goldvip/gvip-manifests -b develop -m default.xml
$ repo sync

 step 3:

$ ./sources/meta-alb/scripts/host-prepare.sh
$ sudo apt-get install libssl-dev

$ source nxp-setup-alb.sh -D fsl-goldvip -m s32g274ardb2 -e "meta-aws
meta-java"

step 4:

bitbake fsl-image-goldvip

Loading cache: 100% |###############################################################################################################################################################################| Time: 0:00:00
Loaded 4931 entries from dependency cache.
Parsing recipes: 100% |#############################################################################################################################################################################| Time: 0:00:03
Parsing of 3345 .bb files complete (3329 cached, 16 parsed). 4949 targets, 289 skipped, 6 masked, 0 errors.
ERROR: No recipes in default available for:
/home/autocore/nxp/nxp-yocto-goldvip/sources/meta-gvip/recipes-core/icedtea/icedtea-native_%.bbappend
/home/autocore/nxp/nxp-yocto-goldvip/sources/meta-gvip/recipes-core/openjdk/openjdk-7_%.bbappend

Summary: There was 1 ERROR message shown, returning a non-zero exit code.



 

0 Kudos
Reply
1 Solution
2,151 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

It seems like the meta-java layer wasn't added to the workspace.

1. Could you check whether you have the meta-java directory in the yocto source directory (it should have been created after the `repo sync` command)? You can do that by running `$ ls ~/nxp-yocto-goldvip/sources/meta-java`.

2. If the meta-java directory does exist, could you check whether this layer is referenced in your conf/bblayers.conf (this should have been configured by the `nxp-setup-alb.sh` script)? You could run `$ cat ~/nxp-yocto-goldvip/build_s32g274ardb2/conf/bblayers.conf | grep meta-java` to check that.

I guess the issue here is that the `nxp-setup-alb.sh` didn't manage to add the meta-java layer in bblayers.conf due to the newline from the setup script command. You could add the entry by yourself, or you could try running again the setup script without any new lines breaks in it: `$ source nxp-setup-alb.sh -D fsl-goldvip -m s32g274ardb2 -e "meta-aws meta-java"`

Thanks,

George

View solution in original post

2 Replies
2,152 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

It seems like the meta-java layer wasn't added to the workspace.

1. Could you check whether you have the meta-java directory in the yocto source directory (it should have been created after the `repo sync` command)? You can do that by running `$ ls ~/nxp-yocto-goldvip/sources/meta-java`.

2. If the meta-java directory does exist, could you check whether this layer is referenced in your conf/bblayers.conf (this should have been configured by the `nxp-setup-alb.sh` script)? You could run `$ cat ~/nxp-yocto-goldvip/build_s32g274ardb2/conf/bblayers.conf | grep meta-java` to check that.

I guess the issue here is that the `nxp-setup-alb.sh` didn't manage to add the meta-java layer in bblayers.conf due to the newline from the setup script command. You could add the entry by yourself, or you could try running again the setup script without any new lines breaks in it: `$ source nxp-setup-alb.sh -D fsl-goldvip -m s32g274ardb2 -e "meta-aws meta-java"`

Thanks,

George

2,141 Views
fenghua_jiang
Contributor IV

Hi George,

    Thank you very much!

regards,

jiang

0 Kudos
Reply