Flexray could not transmit pdu
‎12-04-2024
12:16 AM
376 Views
zyt
Contributor III
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I use two flexray node to connect together, they can both transfer to POC active.
but when I try to transmit pdu from one node, the flag bit MBIF can never be set and status always return busy. The other node can also not get MBIF set.
What might be the proble is?
1 Reply
‎12-04-2024
07:14 PM
346 Views

NXP Employee
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hi,zyt
In order to provide you with better help, please provide more information.
Which version of the LLCE driver are you using? Does your question use any routines?
Do you use custom boards? If not, is it an RDB or EVB board?
BR
Joey