Good afternoon,
I am trying to boot a s32g3-rdb3 board with an sd-card image built from the auto-yocto repo (https://github.com/nxp-auto-linux/auto_yocto_bsp).
Most of the times, especially at the beginning of a new day, the execution of ATF hangs with the following error:
NOTICE: Reset status: Power-On Reset
ERROR: Failed to configure the DDR subsystem
PANIC at PC : 0x000000000000003f
On most days, after a long series of resets, at some point the boot process succeeds and from there on the board usually boots correctly for the entire day.
What could be the cause of this behavior?
I'm using the the sd-card provided in the board's box.
Thank you in advance.
Matteo Zini
已解决! 转到解答。
Hi @Matteo_Zini,
thanks for sharing the test results. With that we can confirm that is not a hardware issue with the DDR.
Can you tell me which version of bsp are you using? Also, are you doing any modifications to the distribution?
The board is new.
I think what happened is that during the first day, with the sd-card image provided on the card I found in the box, it worked without issues. Then I flashed my bsp image on the same card and it worked normally again.
Then on the second day it started behaving like that.
Thanks.