Not able to build Goldvip image and its failing in pkcs_hse . getting below error
Also let me know the link for HSE firmware which has to kept locally while building the image
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/Goldvip/nxp-yocto-goldvip/sources/poky/meta/recipes-devtools/gcc/gcc-cross_10.2.bb:do_populate_sysroot', 'virtual:native:/Goldvip/nxp-yocto-goldvip/sources/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot', '/Goldvip/nxp-yocto-goldvip/sources/poky/meta/recipes-devtools/gcc/gcc-runtime_10.2.bb:do_populate_sysroot', '/Goldvip/nxp-yocto-goldvip/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', 'virtual:native:/Goldvip/nxp-yocto-goldvip/sources/meta-alb/dynamic-layers/core/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', '/Goldvip/nxp-yocto-goldvip/sources/poky/meta/recipes-core/glibc/glibc_2.32.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['gcc-cross-aarch64', 'patch-native', 'gcc-runtime', 'quilt-native', 'pseudo-native', 'glibc', 'linux-libc-headers', 'automake-native', 'libtool-native', 'flex-native', 'mpfr-native', 'xz-native', 'texinfo-dummy-native', 'libmpc-native', 'binutils-cross-aarch64', 'gnu-config-native', 'autoconf-native', 'zlib-native', 'gmp-native', 'attr-native', 'libgcc', 'm4-native', 'gettext-minimal-native', 'bison-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_install
| install: cannot stat '/Goldvip/nxp-yocto-goldvip/build_s32g274ardb2/tmp/work/cortexa53-crypto-fsl-linux/pkcs11-hse/1.0-r0/git/libpkcs-hse.so': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/Goldvip/nxp-yocto-goldvip/build_s32g274ardb2/tmp/work/cortexa53-crypto-fsl-linux/pkcs11-hse/1.0-r0/temp/run.do_install.3433577' failed with exit code 1:
| install: cannot stat '/Goldvip/nxp-yocto-goldvip/build_s32g274ardb2/tmp/work/cortexa53-crypto-fsl-linux/pkcs11-hse/1.0-r0/git/libpkcs-hse.so': No such file or directory
| WARNING: exit code 1 from a shell command.