Enable LLCE support for Linux on S32G( Goldbox)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable LLCE support for Linux on S32G( Goldbox)

1,546 次查看
rital123
Contributor I

We would like to use CAN2ETH feature of LLCE. So need a few information on this:
1>Is this feature enabled for the same?It would be great if you can provide us with guide to use the existing CAN2ETH feature?
2>If No, please let us know how could it be done?
Are there any BSP changes to be done.

0 项奖励
回复
3 回复数

1,244 次查看
salimmulla2021
Contributor III

@Bio_TICFSL 

Is LLCE supported on Linux operating system? If yes where we will get the BSP driver for same?

 

0 项奖励
回复

1,537 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rital123,

 

You can view this appnote for reference:

https://www.nxp.com/docs/en/application-note/AN13423.pdf

 

regards

0 项奖励
回复

1,534 次查看
Aishwarya
Contributor I

@Bio_TICFSL 

CANtoETH process given in this pdf will be used for linux bsp installed Goldbox?

0 项奖励
回复