EB TRESOS LICENSE ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB TRESOS LICENSE ISSUE

417 Views
SURIYA137
Contributor I

Subject: Missing License Error for CAN Module in EB Tresos Tool

Description:

Dear NXP Support Team,

I am encountering a license-related issue while working with the EB Tresos Tool. Upon launching the tool and attempting to configure the CAN module, I receive the following error message:

 Steps Taken So Far:

  1. Verified that the module is required for my configuration.
  2. Checked the License Manager in EB Tresos Tool — the module license is not listed.
  3. Attempted to re-import existing licenses, but the issue persists.

Request:

Kindly assist with the following:

  • Provide guidance on how to obtain and install the required license.
  • Let me know if any additional steps or updates are needed to resolve this issue.

Thank you for your support.

Best regards,
Suriya

0 Kudos
Reply
3 Replies

364 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @SURIYA137 

Thanks for your reply.

From the release notes of SW32G_RTD_4.4_5.0.0_QLP03, it is suggested using the following version EB:

chenyin_h_0-1757555842605.png

I had just tested it with CAN example, the can module could be configured.

chenyin_h_1-1757555941371.png

Would you mind have another trial with EB27.1? it could be downloaded from your NXP account.

 

BR

Chenyin

 

0 Kudos
Reply

379 Views
SURIYA137
Contributor I

Yes, I am working in S32G3.
ANd I already have the RTD SW32G_RTD_4.4_5.0.0_QLP03

0 Kudos
Reply

384 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @SURIYA137 

Thanks for your post.

1. May I know if you are working with S32G3 products? 

2. Seems you are trying the RTD, which version?

 

BR

Chenyin

0 Kudos
Reply