Does the S32R45 support PCIe NVMe SSDs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the S32R45 support PCIe NVMe SSDs?

Jump to solution
1,882 Views
amei_liu
Contributor II

hardware: S32R45 EVB

                Crucial P3 1TB PCIe M.2 2280 SSD

I connect this SSD to the PCI interface of the EVB through an M.2 to PCIE cable.As follow:

11.png

 

After the EVB board is started, enter the following command in the shell interface:

222.png

 

Tags (1)
0 Kudos
Reply
1 Solution
1,810 Views
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

Yes, it does. The connector you are using is configured by default to work as EP, not RC. 

There are a few things to take into account like the clock and the EP/RC configuration in the BSP.

There are more details on how to get that port working as RC here

https://community.nxp.com/t5/Other-NXP-Products/S32R45-Does-PCIe1-work-as-Root-Complex-mode-on-the-S...

Saludos,

Alejandro

 

View solution in original post

0 Kudos
Reply
1 Reply
1,811 Views
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

Yes, it does. The connector you are using is configured by default to work as EP, not RC. 

There are a few things to take into account like the clock and the EP/RC configuration in the BSP.

There are more details on how to get that port working as RC here

https://community.nxp.com/t5/Other-NXP-Products/S32R45-Does-PCIe1-work-as-Root-Complex-mode-on-the-S...

Saludos,

Alejandro

 

0 Kudos
Reply