DCD configuration for S32G274A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCD configuration for S32G274A

1,195 Views
jjysekm
Contributor I

Hello NXP Team,

How to do peripheral configuration in DCD for S32G274A?

Any application notes/user guides against different interfaces (Example SD Card Boot, PLL, MC_ME etc) would be helpful

Thanks

Jeffin

0 Kudos
Reply
1 Reply

1,171 Views
bpe
NXP Employee
NXP Employee

The recommended way to build a DCD is by using S32DS DCD Tool. Explanations
on how to use the tool can be found in the DCD tool howto, which is part of
S32DS installation:

S32DS\help\resources\howto\HOWTO_Use_DCD_Tool_To_Create_A_Device_Configuration_Data_Image.pdf

Integration Reference Examples package offers several ready DCD binaries, refer
to the Bootloader User Manual, which is part of the same package. The software
is available through Flexera, under the S32G2 Reference Software .

 

Hope this helps,
Platon

 

0 Kudos
Reply