Hello NXP Team,
How to do peripheral configuration in DCD for S32G274A?
Any application notes/user guides against different interfaces (Example SD Card Boot, PLL, MC_ME etc) would be helpful
Thanks
Jeffin
The recommended way to build a DCD is by using S32DS DCD Tool. Explanations
on how to use the tool can be found in the DCD tool howto, which is part of
S32DS installation:
S32DS\help\resources\howto\HOWTO_Use_DCD_Tool_To_Create_A_Device_Configuration_Data_Image.pdf
Integration Reference Examples package offers several ready DCD binaries, refer
to the Bootloader User Manual, which is part of the same package. The software
is available through Flexera, under the S32G2 Reference Software .
Hope this helps,
Platon