Change PFE2 MAC address in S32G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change PFE2 MAC address in S32G

115 Views
Sungbhin-Oh
Contributor II

Hi, community.

I am using an S32G-VNP-RDB3 board, building Linux BSP 38.0 to develop PFE and PTP.

 

Is there any way to change the MAC address of the PFE2 on the board?

I'm testing ptp communication between NXP boards and it's not working properly because of the duplicate MAC address.

0 Kudos
Reply
1 Reply

84 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Sungbhin-Oh 

Thanks for the question.

Since you are working with Linux from BSP38, may I know if you ever used the commands in Linux to set the alternative MAC address?

For example, ifconfig pfe2 hw ether $NEW_MAC

 

Best Regards

Chenyin

 

0 Kudos
Reply