Cannot Open the IVT Panel in S32DS When Trying to Generate Boot Image for S32G3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot Open the IVT Panel in S32DS When Trying to Generate Boot Image for S32G3

1,153件の閲覧回数
lihongjun
Contributor III

Dear NXP,

I am trying to generate a boot image for S32G3 using IVT_TOOL of S32DS3.5, according to the steps introduced by AN13750.

I created the S32G3_IVT project, the selected core is Cortex-M7(core #4). The steps are as follow:

Step1

lihongjun_0-1697785573904.png

Step2

lihongjun_1-1697785619779.png

Step3 After Open IVT:

lihongjun_2-1697785855652.png

But after the project has been created, I open IVT view, the IVT tool cannot be open to set boot target, boot device etc., as shown below:

lihongjun_3-1697786150157.png

While other tools, such as DCD, QSPI and DDR can be open.

Please tell me if this is normal or I should modify the project config again?

Thank you.

 

0 件の賞賛
返信
1 返信

1,140件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you share a capture of the behavior you are seeing? The capture you have shared is the enablement of the IVT, but not the IVT window (or the lack of it).

Could be related to the following thread:

S32DS IVT show nothing - NXP Community

Please, let us know.