Cannot Open the IVT Panel in S32DS When Trying to Generate Boot Image for S32G3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot Open the IVT Panel in S32DS When Trying to Generate Boot Image for S32G3

1,151 Views
lihongjun
Contributor III

Dear NXP,

I am trying to generate a boot image for S32G3 using IVT_TOOL of S32DS3.5, according to the steps introduced by AN13750.

I created the S32G3_IVT project, the selected core is Cortex-M7(core #4). The steps are as follow:

Step1

lihongjun_0-1697785573904.png

Step2

lihongjun_1-1697785619779.png

Step3 After Open IVT:

lihongjun_2-1697785855652.png

But after the project has been created, I open IVT view, the IVT tool cannot be open to set boot target, boot device etc., as shown below:

lihongjun_3-1697786150157.png

While other tools, such as DCD, QSPI and DDR can be open.

Please tell me if this is normal or I should modify the project config again?

Thank you.

 

0 Kudos
Reply
1 Reply

1,138 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you share a capture of the behavior you are seeing? The capture you have shared is the enablement of the IVT, but not the IVT window (or the lack of it).

Could be related to the following thread:

S32DS IVT show nothing - NXP Community

Please, let us know.