Boot m7_0 failed on S32G-VNP-RDB2 followed AN13750.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot m7_0 failed on S32G-VNP-RDB2 followed AN13750.

468 Views
chengpei
Contributor III

Hello,

I want to boot A53 from m7_0 on S32G-VNP-RDB2, and I followed the steps in this document <AN13750 Enabling Multicore Application on S32G2>.

After I flashed my binaries to my board, the m7_0 did not even started, as the lauterbach said "running(reset)", which means the core did not start.

chengpei_2-1700753384663.png

Is there something wrong with this "s32g2xx_hse_fw_0.1.0_1.0.5_pb220413.bin.pink"?

Can you give me a blob binary which can boot m7_0 and then boots A53 successfully? 

My Lauterbach flashing script:

chengpei_1-1700753365275.png

My IVT configuration:

chengpei_0-1700752906563.png

Below is my blob.

0 Kudos
Reply
1 Reply

454 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which Bootloader version are you using? Which BSP version are you using? Have you confirmed that your BSP image is working as expected after the required modifications?

Have you confirmed that your HSE image is working? There is a DEMOAPP for HSE that explains the required steps to enable HSE and the usage of pink and blue image.

As for HSE enabled Bootloader, AN13750 details modifications required under the Bootloader source, have you applied the required modifications to the specified source files?

Please, let us know.

0 Kudos
Reply