Hi Team,
I am working on S32G2 based S32G-VNP-EVB hardware. BSP33 images are flashed.
When i flash sdcard image, everything is working fine. I tried to create NOR image from yocto, by adding "flashimage" to IMAGE_FSTYPES.
This image didn't worked when i tried to flash the same on hardware, using S32G Flash tool using UART.
Instead of complete image i tried to flash BL2 + BL31 + U-BOOT (fip.s32-qspi) on target using S32G flash tool. Able to flash and check the binary on flash using the tool, both are same. Still device is not booting from NOR flash.
Could you please tell me the reason for this behavior ?
Do we need to any modifications for NOR in ATF ?
I have presumed as fip.s32-qspi is created, it will be already taken care.
Hi Anish khanna
Thank you for using nxp portal. Hope that you are doing well.
There are another method of generating a flash bootable image from yocto is with using
$ bitbake fsl-image-flash
I have S32g274a-vnp-rdb2 board.i have tested. the image is booting. i have used s32g-Flash-Tool to flash (fsl-image-flash-s32g274ardb2.flashimage). Turn off serial mod and turn on qspi boot mod from changing dip switch after Flashing image.
Regards ,
Tushar