Build NXP Auto Linux Yocto BSP on Windows using WSL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build NXP Auto Linux Yocto BSP on Windows using WSL

Build NXP Auto Linux Yocto BSP on Windows using WSL

This document provides a step-by-step guide to building the NXP Auto Linux Yocto BSP using WSL 2 (Windows Subsystem for Linux) instead of a full virtual machine or native Linux installation. This approach is especially useful for developers working in Windows environments who want a faster and more streamlined way to set up their development environment for platforms like the S32G-VNP-RDB3.

The guide covers everything from installing WSL 2 and configuring system resources, to downloading the BSP, building it with Yocto, and flashing the image to an SD card. It also includes practical tips to help avoid common build issues.

 

标签 (1)
附件
无评分
版本历史
最后更新:
‎05-28-2025 01:27 PM
更新人: