why GD3000 enters low VLS error status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why GD3000 enters low VLS error status

1,573件の閲覧回数
Jack_cheng
Contributor II

I'm testing my own BLDC motor on MCSXTE2BK142 daemon board.  With freemaster runs on PC and MCAT tools could run normally. I MCAT tools enters error status after clicked the ON button. The MCAT shows GD3000 error,as following.

zilong911_0-1666614265338.png

I'm not sure what happens.

My BLDC motor has following parameters,

voltage:DC12V

idle current:0.35A

idle speed:4850 RPM

at rated load:

109 mN.m

current:4.5±15%A

speed:3500±15%

pole-pairs :4

I modified PMSM_appconfig.h file according to my BLDC motor as following,

zilong911_1-1666614914027.png

 

But the same errors happens  repeatly as above.

Any suggestion is appreciated.

Thanks very much.

 

 

I checked the dcb_v_pos voltage ,it's 12.1

 

 

 

For the world u are someone,but for someone u are the world
ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,509件の閲覧回数
JoaquinL
NXP Employee
NXP Employee

Hi Jack,

Low VLS error means the power supply for the gate drives is under voltage. The VLS under voltage threshold is between 7.5 V and 8.5 V. 

Maybe there is something wrong in your HW/SW. Here are some suggestions for you:

  • Check your PWM polarity. Note: the high side is low active and low side is high active.

JoaquinL_0-1667554095809.png

 

  • Increase the deadtime of PWM
  • Check you motor control SW/HW

BR, Joaquin

0 件の賞賛
返信

1,536件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,
I've talked to application team, once they have time they will have a look at your issue.

Best regards,

Peter

0 件の賞賛
返信