sleep mode disable in uja1169

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sleep mode disable in uja1169

1,555件の閲覧回数
Ashik
Contributor I

hi,

how can i disable the sleep mode in uja1169. is it required any factory reset to do that. how to change the SLPC bit value to 1 in uja1169. How to configure the SBC configuration control register (address 74h).

 

Thanks in advance

 

0 件の賞賛
返信
2 返答(返信)

1,520件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

in order to disable Sleep mode (set SLPC bit) you need to program MTPNV cells, here address 0x74. If the device has been programmed previously, the factory presets may need to be restored before reprogramming can begin. Read chapter 7.11 Non-volatile SBC configuration of the device datasheet for more info. 
If using SBC's SDK driver then there is a function to change factory preset value of non-volatile memory.

PetrS_0-1671540666513.png

just set factories.control.slpc accordingly.

BR, Petr

 

0 件の賞賛
返信

1,517件の閲覧回数
Ashik
Contributor I

thankyou for the replay!

0 件の賞賛
返信