s32k144 UART Callback

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32k144 UART Callback

8,332 次查看
heezes
Contributor II

Hello i'm using Uart communication in s32k144 in interrupt mode with the sdk generated by Processor Expert. I'm trying to use the Callback function for receiving data and send data continuously in while loop. The code stops transmitting after 4 bytes and niether does it receives. Code snippet below:

 void ThisIsMyRXCallback(void *driverState, uart_event_t event, void *userData)
{
    PINS_DRV_TogglePins(PTD,(LED15));
}

int main(void)
{
CLOCK_SYS_Init(g_clockManConfigsArr,CLOCK_MANAGER_CONFIG_CNT,g_clockManCallbacksArr,CLOCK_MANAGER_CALLBACK_CNT);
    CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
    INT_SYS_InstallHandler(LPIT0_Ch0_IRQn,&LPIT_ISR,(isr_t *)0);
    LPUART_DRV_Init(INST_LPUART1, &lpuart1_State, &lpuart1_InitConfig0);
    LPUART_DRV_ReceiveData(INST_LPUART1,(uint8_t *)&datas,1);
    LPUART_DRV_InstallRxCallback(INST_LPUART1,ThisIsMyRXCallback,NULL);
    LPIT_DRV_Init(INST_LPIT1, &lpit1_InitConfig);
    LPIT_DRV_InitChannel(INST_LPIT1, 0, &lpit1_ChnConfig0);
    LPIT_DRV_StartTimerChannels(INST_LPIT1,(1<<0));
    PINS_DRV_Init(NUM_OF_CONFIGURED_PINS,g_pin_mux_InitConfigArr);
    PINS_DRV_SetPinsDirection(PTD,(LED15));
    PINS_DRV_SetPins(PTD,LED15);
  /* For example: for(;;) { } */
    for(;;)
    {
        uint8_t data[20] = "Hello World\r\n";
        LPUART_DRV_SendData(INST_LPUART1,(const uint8_t *)&data,strlen(data));
        Delay(500);
    }

}

5 回复数

6,515 次查看
kasundinesh
Contributor II

I was able to solve this issue by using the code below. 

status = UART_Init(&lpuart1_uart_instance, &lpuart1_uart_Config0);

// After calling UART_Init, you need to tell the driver to listen for a single byte
status = UART_ReceiveData(&lpuart1_uart_instance, &g_rx_byte, 1);

At the interrupt service routine.....

void on_byte_received(void *driverState, uart_event_t event, void *userData)
{
   if(event == UART_EVENT_RX_FULL)
   {
      packet_decoder(g_rx_byte);

      // After you got the byte, tell the driver to listen for more bytes. Dont use the UART_ReceiveData. 

     // Use UART_SetRxBuffer insted.
      UART_SetRxBuffer(&lpuart1_uart_instance, &g_rx_byte, 1);
   }
}

Sorry for the late reply

6,516 次查看
heezes
Contributor II

Hi, would like to tell that the issue is resolved it was probably a hardware error.

Regards.

Altamash

6,516 次查看
kasundinesh
Contributor II

HI, I have the same problem. How did you resolve it? Because there is the bug in the driver.

0 项奖励
回复

6,516 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

do you have some data consumer/sender on the other side - like some PC application that is receiving and transmitting data to EVB? 

Jiri 

0 项奖励
回复

6,516 次查看
heezes
Contributor II

Yes I'am manually sending data via a serial terminal Real Term.

Regards.

Altamash.

0 项奖励
回复