processor expert generated empty files in S32DS PA V2.1 SDK 3.0.0 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

processor expert generated empty files in S32DS PA V2.1 SDK 3.0.0 example

1,245件の閲覧回数
bingwang312
Contributor III

I just started to learn examples of SDK 3.0.0 on my devkit MPC5744P, so far i have not got any example working.  an interesting error is, i configured exponents everything, then clicked to processor expert to generate codes, at the first time when i checked some missing .h/.c header files, the folder and files were not there , the second time when i checked then, the folder and files automatically been created, confussing thing is these files are empty. i deleted those empty files, copied same files from another project, then generate code with PE again, these files became empty again. see the pictures below, any suggestion?

bingwang312_0-1639367132318.pngbingwang312_1-1639367168095.pngbingwang312_2-1639367185609.pngbingwang312_3-1639367197192.png

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)