problem on hsrun mode in s32k144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problem on hsrun mode in s32k144

656 次查看
zhangchun
Contributor III

Hello,

the project in the attachment is to activate the HSRUN mode of s32k144, start the timer, and detect the timer function through PTD6. Currently encountering some issues (RUN MODE does not have these issues)

1. The working frequency of ftm3 is configured as 112M, but this configuration has not taken effect

zhangchun_0-1692363649561.png

zhangchun_1-1692363674224.png

ftm0 ftm1 ftm2 are also 48M

 

2. Configure 'Final value', but the timer did not generate the expected timing time

zhangchun_2-1692363795973.png

zhangchun_3-1692363871466.png

 

thanks

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数