problem on hsrun mode in s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem on hsrun mode in s32k144

655 Views
zhangchun
Contributor III

Hello,

the project in the attachment is to activate the HSRUN mode of s32k144, start the timer, and detect the timer function through PTD6. Currently encountering some issues (RUN MODE does not have these issues)

1. The working frequency of ftm3 is configured as 112M, but this configuration has not taken effect

zhangchun_0-1692363649561.png

zhangchun_1-1692363674224.png

ftm0 ftm1 ftm2 are also 48M

 

2. Configure 'Final value', but the timer did not generate the expected timing time

zhangchun_2-1692363795973.png

zhangchun_3-1692363871466.png

 

thanks

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies