phase shifted pwm channels in s32k144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

phase shifted pwm channels in s32k144

527件の閲覧回数
snow3847
Contributor II

Hi, 

I want to generate 2 pwm signals with a 90/180 degree shift between them. I am using s32k144 and the Timer module FTM1 with edge aligned mode.

- Should i use combined channel configuration or independent channel configuration? 

- if both work how can i realise the phase shift with both configurations?

(I could barely find any documentaion with SDK )

 

thank you!

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

507件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

I share with you a demo that perform the modified combined and complementary modes for phase shift and with dead time insertion. It look like this:

_Leo__0-1719444639138.png

I attach the project using S32 Design Studio for S32 Platform v.3.5 and RTD for S32K1 and S32M24x version 2.0.0 including patch P01.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信

494件の閲覧回数
snow3847
Contributor II

Hi,
Thank you for the reply .
From the Project that you sent me i can see that we don't have the same SDK. i have SDK 4.0.1 for S32 DS which looks like this : 

snow3847_0-1719471682375.pngsnow3847_1-1719471704572.png

 

0 件の賞賛
返信

483件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

There is also as reference the AN5303: Features and Operation Modes of FlexTimer Module on S32K and to its respective associated file AN5303SW.

0 件の賞賛
返信