generated code usdhc1.h included in S32 SDK for PA 2.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

generated code usdhc1.h included in S32 SDK for PA 2.0.0

ソリューションへジャンプ
1,850件の閲覧回数
ruudsiebierski
Contributor III

Hi,

I recently found that this generated file is included in SDK code.

C:\NXP\S32DS_Power_v2017.R1\S32DS\S32_SDK_S32PA_RTM_2.0.0\middleware\sdhc\usdhc\usdhc_impl.h

...

#include "usdhc1.h"

...

usdhc1.h is generated code and the name is depending on the Processor Expert configuration settings, I cannot understand it is included in the SDK.

BR,

Ruud Siebierski

ラベル(1)
0 件の賞賛
返信
1 解決策
1,746件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I can confirm this is a bug, so I will report is to SDK development team.

Thank you for reporting this.

Regards,

Martin

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,747件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I can confirm this is a bug, so I will report is to SDK development team.

Thank you for reporting this.

Regards,

Martin

0 件の賞賛
返信
1,746件の閲覧回数
ruudsiebierski
Contributor III

Thank you for looking into it!

0 件の賞賛
返信