can not receive the CAN frame with extended ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not receive the CAN frame with extended ID

Jump to solution
1,696 Views
fedora
Contributor III

Hi team:

     I use the can_pal0 and can_pan2 module in PE , and they can send and receive data with standard ID each other.  Then I change the CAN_MSG_ID_STD to CAN_MSG_ID_EXT,  and CAN ID from 0x01 to 0x10001,  but CAN0 cannot receive data sent by CAN2.

     Here are the codes for CANx initial and send, please help me check them.

 
void CAN0_Init(void)
{
  CAN_Init(&can_pal0_instance, &can_pal0_Config0);
  can_buff_config_t Rx_buffCfg =  {
      .enableFD = false,    
      .enableBRS = false,   
      .fdPadding = 0U,
      .idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD,
      .isRemote = false
  };
 
  can_buff_config_t Tx_buffCfg =  {
      .enableFD = false,                
      .enableBRS = false,               
      .fdPadding = 0U,
      .idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD,
      .isRemote = false
  };
  CAN_ConfigRxBuff(&can_pal0_instance, RX_MAILBOX_CAN0, &Rx_buffCfg, Rx_Filter);
  CAN_ConfigTxBuff(&can_pal0_instance, TX_MAILBOX_CAN0, &Tx_buffCfg);
  CAN_SetRxFilter(&can_pal0_instance,CAN_MSG_ID_EXT/*CAN_MSG_ID_STD*/,RX_MAILBOX_CAN0,0);
  CAN_InstallEventCallback(&can_pal0_instance,&CAN0_Callback_Func,(void*)0);
  CAN_Receive(&can_pal0_instance, RX_MAILBOX_CAN0, &recvMsg_CAN0);
}
 
void CAN2_Init(void)
{
  CAN_Init(&can_pal2_instance, &can_pal2_Config0);
  can_buff_config_t Rx_buffCfg =  {
      .enableFD = false,
      .enableBRS = false,
      .fdPadding = 0U,
      .idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD,
      .isRemote = false
  };
 
  can_buff_config_t Tx_buffCfg =  {
      .enableFD = false,
      .enableBRS = false,
      .fdPadding = 0U,
      .idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD,
      .isRemote = false
  };
  CAN_ConfigRxBuff(&can_pal2_instance, RX_MAILBOX_CAN2, &Rx_buffCfg, Rx_Filter);
  CAN_ConfigTxBuff(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_buffCfg);
  CAN_SetRxFilter(&can_pal2_instance,CAN_MSG_ID_EXT/*CAN_MSG_ID_STD*/,RX_MAILBOX_CAN2,0);
  CAN_InstallEventCallback(&can_pal2_instance,&CAN2_Callback_Func,(void*)0);
  CAN_Receive(&can_pal2_instance, RX_MAILBOX_CAN2, &recvMsg_CAN2);
}
 
CAN2 send to CAN0:
can_message_t Tx_msg = {
.cs = 0U,
.id = 0x10001,    //extended ID,  more than 11 bit
.data[0] = 0xaa,
.data[1] = 0xaa,
.data[2] = 0xaa,
.data[3] = 0xaa,
.data[4] = 0xaa,
.data[5] = 0xaa,
.data[6] = 0xaa,
.data[7] = 0xaa,
.length = 8
};
CAN_Send(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_msg);
 
Thanks!
 
fedora
Labels (1)
0 Kudos
Reply
1 Solution
1,630 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

There is no problem with receiving. The error is that you are not sending an extended frame.

place "CAN_ConfigTxBuff()" before "CAN_Send()"

"

{
can_message_t Tx_msg = {
.cs = 0U,
.id = 0x10001,
.data[0] = 0x20,
.data[1] = 0x21,
.data[2] = 0x22,
.data[3] = 0x23,
.data[4] = 0x24,
.data[5] = 0x25,
.data[6] = 0x26,
.data[7] = 0x27,
.length = 8
};
can_buff_config_t Tx_buffCfg = {
.enableFD = false,
.enableBRS = false,
.fdPadding = 0U,
.idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD
.isRemote = false
};
CAN_ConfigTxBuff(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_buffCfg);
CAN_Send(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_msg);
u1_printf("CAN2 send: 20 21 22 23 24 25 26 27\r\n");

"

View solution in original post

0 Kudos
Reply
6 Replies
1,670 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

Could you please share the project so that i can test it for you.

0 Kudos
Reply
1,662 Views
fedora
Contributor III

Thanks for your help!

Please find attached that s32k144 CAN testing project.

If the CAN_MSG_ID_STD macro is used, the CAN0, CAN1 and CAN2 can communicate with each other, but replace CAN_MSG_ID_STD with CAN_MSG_ID_EXT cannot receive any data.

Thanks again!

 

Fedora

0 Kudos
Reply
1,649 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

I test flexcan0 with pcan and i can see no problem on myside.

Senlent_0-1749453463329.png

 

But I do find some issues with your flexcan settings.

The sampling point for flexcan0 is 75%, but the sampling points for flexcan1 and flexcan2 are

87.5%, which may cause communication failure.

 

It is recommended that you first use a PC tool such as PCAN to ensure that each

FLEXCAN instance is working properly.

0 Kudos
Reply
1,642 Views
fedora
Contributor III

Thanks, Senlent.

In my project, I hope CAN2 can send the following data that  ID is 0x10001,  so it's an extended frame;  

Expected to the CAN0 can get ID 0x10001 as well , but the ID received by CAN0 is 0x01,  why?

can_message_t Tx_msg = {
.cs = 0U,
.id = 0x10001,
.data[0] = 0x20,
.data[1] = 0x21,
.data[2] = 0x22,
.data[3] = 0x23,
.data[4] = 0x24,
.data[5] = 0x25,
.data[6] = 0x26,
.data[7] = 0x27,
.length = 8
};

fedora_0-1749465290024.png 

extended frame format

 

0 Kudos
Reply
1,631 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

There is no problem with receiving. The error is that you are not sending an extended frame.

place "CAN_ConfigTxBuff()" before "CAN_Send()"

"

{
can_message_t Tx_msg = {
.cs = 0U,
.id = 0x10001,
.data[0] = 0x20,
.data[1] = 0x21,
.data[2] = 0x22,
.data[3] = 0x23,
.data[4] = 0x24,
.data[5] = 0x25,
.data[6] = 0x26,
.data[7] = 0x27,
.length = 8
};
can_buff_config_t Tx_buffCfg = {
.enableFD = false,
.enableBRS = false,
.fdPadding = 0U,
.idType = CAN_MSG_ID_EXT,//CAN_MSG_ID_STD
.isRemote = false
};
CAN_ConfigTxBuff(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_buffCfg);
CAN_Send(&can_pal2_instance, TX_MAILBOX_CAN2, &Tx_msg);
u1_printf("CAN2 send: 20 21 22 23 24 25 26 27\r\n");

"

0 Kudos
Reply
1,613 Views
fedora
Contributor III

Thanks, Senlent!

After testing, your method is correct.

Before calling Can_send, Tx buffer needs to be reinitialized.

 

0 Kudos
Reply