Will S32V automatically send its ID by CAN or ethernet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Will S32V automatically send its ID by CAN or ethernet?

809 次查看
Da2
Contributor I

Hello friends,

Will S32V automatically send its ID by CAN or ethernet?

BRs 

Yuan Da

标签 (1)
0 项奖励
回复
1 回复

771 次查看
yangruihero
NXP Employee
NXP Employee

Dear Da:

For CAN function, S32V can support “Controller Area Network (FlexCAN)”(please refer to Chapter 40 in S32V234 Reference Manual);

for Ethernet, S32V can support “10/100/1000-Mbps Ethernet MAC (ENET)”(please refer to Chapter 43 in S32V234 Reference Manual);

For S32V UNIQUE_ID, they are located in S32V_Fuse.

S32V FlexCAN and ENET IP will not use UNIQUE_ID directly, because they are just hardware interface, UNIQUE_ID can be used by software.

By the way, we have not heard any CAN software protocol stack or Ethernet software protocol stack will use IC’s ID.

You can check information about CAN-ID or Ethernet MAC address(IP address) from website.

Thanks.

0 项奖励
回复