Why does the network bandwidth of LWIP application not match?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does the network bandwidth of LWIP application not match?

2,245 Views
A-Jay
Contributor III

Hi,

I used the Example program to test the network bandwidth through JPerf Application. The Example program set the bandwidth speed of 1G, but the default initial bandwidth speed can only run to 2Mbits/sec. After adjusting the configuration of the lwipopts.h file, now it can run to 45Mbits/sec, which still does not match the set bandwidth.

MCU: S32R45, M7

System: FreeRTOS

TCP/IP: lwip

Hope to be able to answer!

Attached is the lwipopts.h file.

AJay_1-1674876637264.png

 

AJay_0-1674876574171.png

 

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

2,142 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @A-Jay 

The performance was not good enough as you can see, unfortunately. We will try to improve it in next S32R release.

Best Regards,

Nam

0 Kudos
Reply